Part Number: BOOSTXL-DRV8323RH Other Parts Discussed in Thread: LAUNCHXL-F280049C , , C2000WARE-MOTORCONTROL-SDK , BOOSTXL-DRV8320RS , C2000WARE Hello,
I've purchased a LAUNCHXL-F280049C and a BOOSTXL-DRV8323RH, and also have a DRV8301-HC-C2-KIT to…
Part Number: BOOSTXL-DRV8323RH Hi,
with FAST and HALL both enabled, by default I should run either HALL or FAST right ?
if I select ESTIMATOR_MODE_FAST, under MOTOR_ALIGNMENT state, it's call HALL_setForceAngleAndIndex, which is use to calculate thetaHall_rad…
Hi Danny,
Danny Chan said: 2. my understanding is Over-current happened, faultMtrNow changed fall into line 34 change flagRunIdentAndOnLine to FALSE
You are correct, apologies for the confusion.
Danny Chan said: this is my understanding, UNLESS…
Part Number: BOOSTXL-DRV8323RH Other Parts Discussed in Thread: LAUNCHXL-F280025C , DRV8323
Hi,
Can anyone help to review my schematic which's based on LAUNCHXL-F280025C + BOOSTXL-DRV8323RH combo but
1. MCU replaced with 280023PTSR 48 Pins
2.…
Part Number: BOOSTXL-DRV8323RH Other Parts Discussed in Thread: TMDSCNCD28035 , , LAUNCHXL-F280049C , MOTORWARE , LAUNCHXL-F280025C , TMS320F280025C , INSTASPIN-BLDC , C2000WARE-MOTORCONTROL-SDK , C2000WARE , CONTROLSUITE Hi Team,
I am very new to this…
Part Number: BOOSTXL-DRV8323RH Hi,
I would like to know what's caused the IsRef_A is limited and where can I change its upper limit ?
running SPEED CONTROL MODE
motorVars_M1.flagEnableCurrentCtrl = 1 motorVars_M1.flagEnableSpeedCtrl = 1
when…
Part Number: BOOSTXL-DRV8323RH Other Parts Discussed in Thread: LAUNCHXL-F280025C , DRV8353RS-EVM Hi everyone,
I have issues to get the build 1 running.. Launchpad LAUNCHXL-F280025C is prepared as described. BOOSTXL-DRV8323RH with capacitors populated…
Yanming Luo said: The minimum setting speed by POT is limited to a value, USER_M1_POT_SPEED_MIN_Hz in the project.
yes, I set USER_M1_POT_SPEED_MIN_Hz to 0 for the test
Yanming Luo said: BTW, the sensorless-FOC can't run the motor well with 1 HZ…
Part Number: BOOSTXL-DRV8323RH
Hi,
Can anyone help to explain why MOTOR_ALIGNMENT section called once only ? If enable the onboard POT and use it to change speedRef_Hz as throttle, when system start :
1. set flagEnableRunAndIdentify to 1
2. motorState…
Part Number: BOOSTXL-DRV8323RH Other Parts Discussed in Thread: MOTORWARE Hi,
is SPRUHJ1I the latest / updated document for MotorSDK ? I am bit confuse the document is mixed with both MOTORWARE and MOTORCONTROL-SDK right ?
for instance, on page…