Part Number: BOOSTXL-DRV8323RH
Hi,
HALL + Current Control mode
don't know why once isSet_A reached 0.15, system out of control.
0:03 HALL estimator + Current Control mode start, isSet_A set to 0.09 0:05 motor start, speed_Hz = 6.8 still under…
Part Number: INSTASPINFOCMOTORWAREGUI What changes must be made to the DRV-8323RS projects in order to use a launchxl-F28069M with a DRV-8323RH?
[FAQ] BOOSTXL-DRV8323RS and BOOSTXL-DRV8323RH InstaSPIN and MotorWare support - C2000 microcontrollers forum…
Part Number: BOOSTXL-DRV8323RH Other Parts Discussed in Thread: DRV8323 Hi,
Can I simply
EN pin direct connect to 3v3 MODE pin direct connect to GND GAIN pin connect to GND via 47k resistor
like in HAL_enableDRV function
GPIO_writePin(obj…
Part Number: BOOSTXL-DRV8323RH Other Parts Discussed in Thread: LAUNCHXL-F28027F , , MOTORWARE , DRV8305 , DRV8323 I wish to use the hardware controlled version ie: BOOSTXL-DRV8323RH paired with a LAUNCHXL-F28027F Launchpad. The doc below indicates that…
Part Number: BOOSTXL-DRV8323RH Other Parts Discussed in Thread: DRV8323 We are exploring DRV8323 + MSP – EXP430F5529LP for a requirement. It is a sensored requirement.
Which GUI tool is suitable for it?
Thank you.
Please have a look at the links below that have a similar question as you.
https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1118537/tms320f280025c-unable-to-use-hall-starter-motor/4154188#4154188…
Part Number: BOOSTXL-DRV8323RH Other Parts Discussed in Thread: MOTORWARE , LAUNCHXL-F28069M , , DRV8323R , DRV8323 Hi,
I bought the following two boards: BOOSTXL-DRV8323RH and LAUNCHXL-F28069M. Now, there are no comming with motorware for the DRV8323RH…
Part Number: BOOSTXL-DRV8323RH Hi,
I am working on the HALL to FAST smooth transition issues and discovered both speedRef_Hz and speedEST_Hz was out of sync.
when running under FAST estimator + Current Control mode, set IsRef_A to 2.0, I have both…
Part Number: BOOSTXL-DRV8323RH Other Parts Discussed in Thread: LAUNCHXL-F28069M , , DRV8323 , MOTORWARE , BOOSTXL-DRV8323RS Hello,
I am trying to spin a BLDC Motor (Trinamic QBL 4208-61-04-013) with the LAUNCHXL-F28069M and the Booster Pack: BOOSTXL…
Part Number: BOOSTXL-DRV8323RH Hi Team,
Customer would like to know the difference between VDS protection and VSENSE protection of DRV8323RH. Both of them obtain current by collecting voltage. Are these two functions repeated, or are there other uses…