Part Number: BOOSTXL-LMG2100-MD
Hi,
Same question as below which was never really resolved... Can you at least provide me the PDF of the sch over E2E?
https://e2e.ti.com/support/motor-drivers-group/motor-drivers/f/motor-drivers-forum/1526178/boostxl…
Part Number: BOOSTXL-LMG2100-MD Other Parts Discussed in Thread: LAUNCHXL-F28P65X Tool/software: Can you add PDF schematic file to BOOSTXL-LMG2100-MD page? Currently only Altium design files are available, which are not as convenient to reference.
Thanks…
Part Number: BOOSTXL-LMG2100-MD Other Parts Discussed in Thread: LAUNCHXL-F28379D Tool/software: I am investigating a solution where I want to use the BoostXL-LMG2100-MD in combination with a launchXL-F28379D. The datasheet mentions that this version…
Part Number: BOOSTXL-LMG2100-MD Other Parts Discussed in Thread: LAUNCHXL-F28P65X , Tool/software: Hello,
Setup
MCU board: LAUNCHXL-F28P65x
Power stage: BOOSTXL-LMG2100-MD (GaN)
Motor: 48 V, 10 A nominal, 10 poles
Sensors: None…
Part Number: BOOSTXL-LMG2100-MD Tool/software: Hello.
I checked the following on TI homepage.
"High efficiency (99.3% peak) at 40kHz PWM enables operation at 25°C ambient and up to 27ARMS continuous current without heat sink."
I am trying to design…
Part Number: TIDA-010936 Other Parts Discussed in Thread: BOOSTXL-LMG2100-MD , , LAUNCHXL-F28P65X , LAUNCHXL-F280039C , C2000WARE Tool/software: Hi team,
Is it possible to use F28388D launchpad for TIDA-010936. It's for using BoostXL-LMG2100-MD which…
Hello,
With only the Launchpad connected after starting IPG-UI:
all the same jumpers are in place (everything but RTS & CTS)
I see the Green LED
The blue "USB2ANY" banner flashes
"Hardware Not Connected" and red circle remain at the bottom…
Hi James,
In the BOOSTXL-TPS650861 User's Guide we recommend a specific firmware update program but it looks like download page is under maintenance at the moment. I will send the program to Ben Su since he has also come forward on this matter in this…
GL,
Thanks for posting on the MD forum!
Could you highlight in schematic what you mean by this statement: "However it seems BoostXL-DRV8320rs use of shunt LP input filter masks over LAUNCHXL-F280049C XDS110 isolation barrier issues"
Regards,
…