Hello Frank, Thank you for posting to the MD forum! The DoC file for the BOOSTXL-DRV8301 can be found here: http://www.ti.com/lit/pdf/sszq143
The DoC file for the LAUNCHXL-F28069M can be found here: https://www.ti.com/lit/pdf/sszq090
Was this what…
Part Number: DRV8323R Other Parts Discussed in Thread: LMR16006 , Dear, MD support team,
I am designing Motor control board, I use DRV8323RH (hardware interface) for gate driver but I have some concerns below:
1, With configuration pins of DRV: MODE…
Hello Pedro,
Thanks for posting to the MD forum. I appreciate the info here, you mentioned you are using the BOOSTXL-DRV8323RH EVM, are you running your own customer firmware to commutate the motor?
Based on the waveforms it doesn't look like this…
Vishwambhar,
Thanks for posting on the MD forum!
I can comment on the two BLDC options above and then hand the post off to the other two teams for comment on the Brushed solution and the C2000 solution.
2) The BOOSTXL-DRV8301 kit supports up to…
Hello Adam
I made a query to Texas Instruments to know which equipment was the right one (I attached the post), in which it said that I needed the control to be able to brake the engine in case of external acceleration, they replied that although, I…
Gonzalo,
Thanks for posting on the MD forum!
The DRV8320 EVM will work with the MSP430F5529 and does have sensored code (with hall sensors) available. The GUI has only duty cycle control but unfortunately not a speed loop or active braking.
That…
Tuan,
Thanks for posting on the MD forum!
The DRV8332 is an older part, it was created before our more recent parts which incorporate things like 3xPWM control.
For example, a similar part that's newer and has 6x, 3x, or 1x PWM modes is the DRV8320…
My motor :
user_mtr1.h:
//! \file /solutions/universal_motorcontrol_lab/common/include/user_mtr1.h
//! \brief Contains the user related definitions
//! This file is used for each device includes F28002x, F28003x, F280013x,
//! F280015x…
Part Number: C2000WARE-MOTORCONTROL-SDK Other Parts Discussed in Thread: C2000WARE , BOOSTXL-DRV8323RS , DRV8323 , CSD88599Q5DC Hi team,
Here's an issue from the customer may need your help:
Environment is as follows:
power supply:12V/100A
Code…