Part Number: ADS7138-Q1 Other Parts Discussed in Thread: ADS7128 , BP-ADS7128 Tool/software: Hello experts,
Is there any requirement on Slew rate or voltage ripple requirement for AVDD/PVDD? (e.g. slew rate <5V/us, ripple < 20mV or something)
Thanks…
Part Number: ADS7128 Other Parts Discussed in Thread: , ADS7830 Tool/software: I have two questions regarding the ADS7128:
On page 15 of the ADS7128 datasheet, the ADDR pin (for configuring the I2C address) is shown with a pull-up to the DECAP pin…
Part Number: ADS7138-Q1 Tool/software: Hello experts,
My customer is drawing schematic for ADS7138-Q1 and they are referring to BP-ADS7128 Evaluation board | TI.com as a start point of their design.
Then, they have questions about details fo resitor…
Hi Christopher,
This was taken with the BP-ADS7128 evaluation module, and that source code is not available to share publicly. I'm not familiar with the I2C utility that you're using, so I can't say for certain what it translates to.
Perhaps you can…
Part Number: ADS7128 The ADS7128 data sheet says the I2C address selection resistors should be connected between the DCAP pin and ground. The schematic diagram in the BP-ADS7128 BoosterPack Plug-In Module User's Guide shows the I2C address selection resistors…
Hi Yong,
Sure. Below is what it would look like.
If you don't have access to hardware yet and would like to test your software, there is an ADS7128 booster pack EVM available for purchase. See the link below. This board is intended for use with the…
Part Number: TLA2518 Other Parts Discussed in Thread: BP-ADS7128 , ADS7128 , ADS7038 Dear Sirs,
I am looking for TLA2518 EVM reference schematics but only ADS7038Q1EVM-PDK is available.
In the user guide, the RC setting of EVM is 1K and 330p.
…
Hello Art,
Do you type the wrong devices number?
Art Kay said: The ADS7138 is a superset of the ADS7128. Every register that is in the ADS7128 is also in the ADS7138, but the ADS7138 has registers and functionality not in the ADS7128
I notice that…
Part Number: ADS7128 Hello,
Where can I find the SW driver for the ADS7128 that is used by the GUI demo in with the evaluation kit BP-ADS7128 BoosterPack.
Thanks