Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: ENERGIA Hello, I'm trying write a control loop in python using a Real-time operating system (RTOS). I want output voltage setpoints to a DAC at ~10kHz. The voltage outputs are single values…
Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: DAC11001B Hi there,
We are debugging DAC11001 for our project. we use EXP432E401Y MCU for controlling DAC11001 output. But we do not have the EXP432E401Y original code/project, could you please…
Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: MSP-EXP432E401Y Hi,
The customer purchased two products, one for BP-DAC11001EVM and one for MSP-EXP432E401Y. When the two products are used together, the customer follows the instruction manual…
Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: DAC11001B Hi Team,
Can you explain what is the purpose of the U10 circuitry below?
Thank you,
Regards,
Marvin
Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: DAC11001A Hello, we Need to know the dimensions of the BP-DAC11001EVM, and also the current consumption on each supply voltage.
Thnak you
Michel Janz
Part Number: BP-DAC11001EVM I am designing a pcb and would like to place the DAC but for this I require design files of the following board: BP-DAC11001EVM can you please assist.
Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: REF6250
Hi there,
I have bought DAC11001EVM and MSP-432E401Y demo. The power-up sequence and value as below.
VCC: +9V
VSS: -9V
VDD: +5V ( same power with VIO )
VIO: +5V
VREF_PWR…
Part Number: BP-DAC11001EVM
Hi there,
Please help to check if below SPI WRITE process is right. ( using GUI write 01H register 00FA00 ), Also, please help to let me know the read process.
When I send write 01H register for 00FA00 data, I set up…
Part Number: BP-DAC11001EVM I am trying to measure the glitch from the BP-DAC11001EVM. I set the software to LDAC, and I'm driving the LDAC with a separate microcontroller. This way I can cue up the code I want to write in software, and then trigger the…
Part Number: BP-DAC11001EVM Other Parts Discussed in Thread: UNIFLASH , EK-TM4C1294XL Hi team,
I got a question from customer.
CASE.docx
Thank you very much for your help.
Best regards,