Part Number: BQ2002 Other Parts Discussed in Thread: BQ25172 , , LM317 Tool/software: Hi,
I'm designing a charger using the BQ2002 family for a 3×AAA NiMH battery pack (~3.6 V). I want to power the circuit directly from a 5 V USB Type-C source (standard…
Part Number: BQ2002 Hi Team,
My customer have followed DV2002L2/TL datasheet for reference design with no major changes. The IC doesn't start fast charging until thermistor is heated. They have experimented all the pins as per state diagram in BQ2002…
Part Number: BQ2002 Hi,
I would like to ask you about how to use the BQ2002/F device. (question 1) Is it necessary to disconnect the supply voltage to this device once when connecting another battery and charging from the beginning after detecting the…
Part Number: BQ2002 Other Parts Discussed in Thread: BQ25172 Hello,
Do we have a waveform or plot that shows the battery charge profile of the BQ2002?
Something similar to Figure 7-1 or 7-2 of the BQ25172: https://www.ti.com/lit/ds/symlink/bq25172…
Part Number: BQ2002
Hi team,
My customer is looking for the charger IC which is similar to DS2715 from ADI.
Do we have such a battery charger IC? (NiMH, 2 cells support)
Best regards,
Shunsuke Yamamoto
Part Number: BQ2002 Other Parts Discussed in Thread: BQ25172 Hi team,
My customer would like to design BQ2002 because of some reason.
The battery material is NIMH and max working voltage around 1.52V. 1cell design only.
And the question is they…
Part Number: BQ2002 Hi,
I would like to ask you about the state transition diagram in Figure 2 of the BQ2002/F and BQ2002E/G datasheets. (question 1) The conditions for shifting from trickle charging to recharging are described as VCC for BQ2002/F and…
Part Number: BQ2002 Other Parts Discussed in Thread: BQ25171-Q1 Hello,
I am new to chargers and I have to solve 3 cell NiMH charging from USB for MSP430. The final charge voltage of the three cell should not exceed 3x1.3V. There is no high expectations…
Part Number: BQ2002 Hi team,
Datasheet says; For PVD (TM = low or mid), a decrease of 2.5mV ±2.5mV terminates fast charge . The PVD and -∆V tests are valid in the range 1V < VBAT < 2V.
Does it mean that "VBAT is lower than any previously measured…
Part Number: BQ2002 Hi team,
What are the concerns when charging NiMH with bq2002 at 0.1C?
Will it not be possible to detect full charge?
Best Regards,