Part Number: BQ2002 Hi
The input power is MICRO USB 5V/0.5A, the charging current is about 200mA,The battery is 2 Ni-MH batteries in series 1.How to set the full charge voltage? 2.How to do overcharge and overdischarge mechanism? Because it will be…
Hi Bill,
Thanks very much for your answer.
I have tried to set the resistor network as RB1=100K, RB2=100K, that means 100k/100k=2 cells -1, but it doesn't work.
when I power up the board, the charge LED is off. the voltage of the BAT+ is around…
Part Number: BQ2002 Hi,
I would like to use the BQ2002 to recharge one 9V Ni-MH rechargable battery (NH22-175 Energizer 9V http://data.energizer.com/pdfs/nh22-175.pdf ).
Most nine-volt batteries are constructed of six individual 1.5V cells enclosed…
Part Number: BQ2002 Other Parts Discussed in Thread: LM317 Hello
My customer have NI-MH battery charger demands, input 5V, 3 NI-MH battery, I find Ti just have BQ2002x for NI-MH charger, but havn't find typical SCH of BQ2002, Could you provides reference…
Part Number: BQ2002 Hello guys,
One of my customers is considering using BQ2002 for their new products.
They have a question about BQ2002 charging method as the follow. Could you please give me your reply?
Q. Does TI recommend to use Negative Delta…
For the eval schematic, how do I control the current delivered to the battery? Is it by adjusting the Vout and Vadj resistor values?
I need an output of 550+ mA which values should I tamper with to obtain that value?
Can I use any other diodes and PNP…
Part Number: BQ2002 Hi,
We got a question from the customer about bq2002. Could you help us?
[Question] - They assume the recommended fast-charge current is spcified in table 1 which is "Corresponding Fast-Charge Rate". Is this their understnading…
Part Number: BQ2002 Hi
Our customer uses BQ2002D and measured on their board. However it does not work as expected.
It sometimes stop fast charge. Also CC voltage become low when it stops.
I have some question regarding to this phenomenon.
1…
Part Number: BQ2002 Hello,
If customer wants to use primary cell and secondary cell mixed in charger, is there any protection method not to charge primary cell?
Customer wants to protect only primary cell when primary cell and secondary cell are…