The bq34z100-G1 should work with the bq24401 charger. They do not communicate with one another, but the gauge should detect charge termination after the delta criteria have been met. You can still use the bq2014H device, although applications support…
Other Parts Discussed in Thread: BQ2014H , BQ2002C , BQ2002 Hi, I'm using a set of bq2002C and bq2014H for charging and measuring (respectively) the capacity of 6 (2000mAh) Ni-MH batteries. The batteries are being charged at the expected rate for C/2,…
We do actually have a few NiCd/NiMH gauges, although they are quite long in the tooth due to the popularity of Lithium.
Try bq2013H, bq2014H, and bq2016. They are all single-wire communication.
We also have the bq2060A which offers multi-chemistry…
Deckerg,
The bq2010EVM is not available. The dip-packaged version of the IC used on this module hasn't been around for some 10 years. The software you reference requires a special interface to the computer RS-232 port and it was built as part of the…
Other Parts Discussed in Thread: BQ27510 I have written the firmware to program the BQ27510 from the three page flow chart from Going to Production with the bq2750x. However, every time I read register 0x66 to see if the data=0x00 I get the data to equal…