Part Number: BQ2026EVM Hi,
This mail is regarding BQ2026 IC of TI. Request you to address the below queries. 1) BQ2026EVM , what are the components this Kit contains? Does it include Reva board along with EV2300 HPA002 interface board ? 2) If it doesn…
Hello Shashi,
1. VPUP can be from 2.65V to 5.5V. So 3.3V shouldn't be a problem.
2. As indicated in the datasheet, Rpup is 5K ohm
3. How does the device respond when you issue a reset pulse for t RST duration?
4. Can you show the waveform for the reset…
Chime Xia,
To answer your questions:
1. The 12V pulse should be issued for each byte (Figure 8 on Page 9 of the datasheet). Each byte is written to the onboard cache, then SDQ is pulled up to 12V for at least 480us. This should be a single pulse.
2. The…
Hi Praveen,
Thanks for the super quick response. I didn't realize that and sent samples of the BQ2026 and the EV2400 to my customer. I did just learn that the authenticators have their own software that is not part of BQStudio:
https://www.ti.com…
Just posted my success connection to someone may need help same with me. (not Software engineer)
>> Hardware <<
I connected BQ2026EVM to EV2400 thru PORT3(HDQ)
>> Software <<
You need to
1) update EV2400 firmware to v0.32
2) i…
Part Number: BQ76930EVM Other Parts Discussed in Thread: BQSTUDIO , EV2400 , BQ76930 , BQ78350-R1 Hi all,
i have some questions about BQ76930EVM:
1) I want to execute a cycle life test on a battery module made by 8 cells using BQ76930EVM and BQSTUDIO. The…
Hi Anthony, (Sorry for the long and somewhat late reply!)
Yes, for development using the bq34z100-G1, you'll need an EV2300 or EV2400 adapter to work with the chips. This is because TI's advanced Impedance Track fuel gauges require a lot of configuration…