Part Number: BQ2057W Other Parts Discussed in Thread: BQ2057 , MSP430F5529 Good evening....
I am using a BQ2057W (8.4V) part and want to take the STAT output to an MSP430 input....The MSP430 is a 3.3V part.....The STAT will be driven, low, high or tri…
Part Number: BQ2057W Can someone explain to me why I cannot turn the input voltage above 10.2V to charge my 8.4V batteries? I am using high side sensing (100 mOhms) with a P-FET. My input current is 1.4A and output is charging at about 1A (see Figure…
Part Number: BQ2057W Hi.
I design a charger batteries board. I use 2 cell batteries 18650 3.7V@3.400mAh.
Charging is Ok. But when I remove adapter +9V, always have a leakage current 4mA to BQ2057W circuit from batteries (VBAT). It makes the remain…
Part Number: BQ2057W Other Parts Discussed in Thread: BQ2057 , CSD25404Q3 We are Using BQ2057 battery charger IC in our product to charge the 8.4V battery through 9V-1A adapter. As per the datasheet to enable/disable the charging process, we used AO4409…
Part Number: BQ2057W Hi all,
I have used BQ2057W in my design for batter charging application. I have used battery with NTC thermistor.
I have used reference design given in TI's BQ2057W datasheet. For Battery Temperature Monitoring, two Resistors…
Part Number: TPS62135 Other Parts Discussed in Thread: BQ2057 , , TPS62136 , BQ24103A , BQ24133 Good morning... I am using the above buck converter to feed the above battery charger. This is being done through a pair of PFETs DMP2007UFG-7. The system…
Part Number: BQ2057W I am using this IC to charging 7.2V, 2200mAHr li ion battery.
I m facing following problems
1. O/p vtg. is 9.5V
2. For current controlling, use 0.2 Ohm resistance but when I measure the current, it shows 1.2 A
Attaching…
Part Number: BQ2057W
Hi,
I am using BQ2057W to charge a 7.4V 10Ah 2S Lithium Ion Battery with 12V charger and 1A Charge Current. Attached is the circuit for reference. I have the following issues:
1. When on Battery (12V Charger NOT Connected),…