Part Number: BQ2060 Other Parts Discussed in Thread: BQSTUDIO , EV2400 Hello All,
I was wondering if anyone else here has seen this scenario on battery packs using the BQ2060 - after an event like a battery pack going overtemp - subsequent queries for…
Part Number: BQSTUDIO Other Parts Discussed in Thread: BQ2060 , EV2400
Hello,
I'm using the EV2400 to connect to the SMBUS on some battery packs that have the BQ2060 - is there a way to customize the profiles of bqStudio for the BQ2060's? I also…
Part Number: BQ2060 My name is Denny Beasley and I work for NPC (national power company) and we have our automated test program platform for battery products we manufacture. We have a customer with a custom battery pack using the BQ2060A and I need to…
Part Number: BQ2060A Other Parts Discussed in Thread: BQ4050 , BQ2060 I have a battery with a fuel gauge BQ2060A.What is the ambient temperature not to be exceeded for the calibrate of the capacity and for the learning?
At 35°C, the calibration offset…
For many years this value would measure <10 but now after the redesign of the PCBA it now measures up to 50 while all other cell calibration factors remain under 5. The measurements of the individual cells and the battery pack voltage are as expected…
Other Parts Discussed in Thread: BQ2060 How is the value for Current Taper Threshold at EEPROM location 0x4e set? The value and units aren’t well documented in the datasheet.
How does the programmed value 0x12 convert to 200 mA?
Is the value fixed…
Other Parts Discussed in Thread: BQ2060 10 year old bq2060 based design with large production base in the field shows 150% charge at times when new assemblies reach final test in production. Lead acid (2ea of 12V 28Ah in series) batteries are fully charged…
Other Parts Discussed in Thread: BQ2060 Hello,
I'm looking for some help with the bq2060 battery fuel gauge. My company was contracted to resurrect a short production run of a Li-Ion battery previously designed with this older technology for fuel gauging…
Hi Wyatt,
Here is the customer response:
"Yes we do understand that PEC byte is combination of the whole packet of 5 bytes. As in the screenshot taken from bq2060 we requested remaining capacity whose command is 0x16 and reply packet is 0x16, 0x01…