Part Number: BQ21061 Hi team,
In customer side we met a strange issue. Customer use BQ21061 and its TS function. They found that TS voltage is only 18mV, and charging can't work. After reading the register, STAT0=0x01, STAT1=0x00, STAT2=0x01, which means…
Part Number: BQ21061 can we use BQ21061 instead
, IN present design the ADCIN pin is not be used.
Are there any potential risks for battery charge or discharge is different voltage , like low voltage(2.5V/2.6V/2.7V).
Part Number: BQ21061 Hi team,
My customer is using our BQ21061 and they have some questions about it.
How do we trigger our Chare_done ? Is it IBAT < ITERM which is shown as below figure orit is triggered by when the VBAT achieved Battery Regulation…
Part Number: BQ21061 Hi team,
My customer has two questions about I2C setting.
.
1. Can they just use the BQ21061YFPR default register setting to bring up or they need to change it?
2. Is there any sample code for BQ21061YFPR with I2C interface?
Part Number: BQ21061 About TI battery charger BQ21061YFPR, I have the following questions during product validation. Kindly advise it. Thanks.
1、REF the datasheet “2b00 = PMID powered from BAT or VIN if present”, does it means:
if Vin present…
Part Number: BQ21061 Dears,
One of my customer is using the BQ21061 for a wearable device, and they want to have the status of Fast charger flag, seemed we do not have this status register? and if yes, is there a way to know the charger is in the fast…
Part Number: BQ21061
Hi team,
My customer has some doubts about the low power mode of BQ21061. Does the battery still powers up PMID pin during low power mode?
They have the question because of BATOCP is off during low power mode. Sorry. Not very familiar…
Part Number: BQ21061 Hi Sir,
We have a question about bq21061 in low power mode
Please see highlight below, does it depend on the HW reset timer?
Thanks, Ian.