Part Number: BQ24010 Hi Team,
My customer would like to use the BQ24010 on an automotive-related product, They need to know this device has or not to pass the certification for IEC/EN 60950-1 or IEC/EN 62368-1.
Could you please check and reply to me as…
Part Number: BQ24010 I would like to use the BAT sense input to boost the OUT voltage by approximately 50mV to account for cable losses in a charging application. I am using a 10K/1M voltage divider between OUT and BAT. The values are intentionally high…
Part Number: BQ24010 Other Parts Discussed in Thread: BQ24076 , BQ24040 , BQ24100 Hi, I want to use BQ24010 for my design. From the application circuit, it is noted that the Charge current output (Pin) is connected to both Battery and Load together, where…
Part Number: BQ24010 Hi,
I am using BQ24010DRCR charging IC in my application. I have connected 3.7V Li-ion battery to VCC_VBAT. I am giving 12.8V as input. Below i have included circuit design. My external circuit connected to VCC_VBAT consumes maximum…
Other Parts Discussed in Thread: BQ24010 Hi,
I have a question regarding to BQ24010.
Could you confirm me that BQ24010 don't have charge TIMER ?
Thanks a lot,
Best Regards,
David
Part Number: BQ24010 I am using the BQ24010 to charge a single cell 4.2v Lithium Ion battery. The battery is being used in an Intrinsically Safe environment so it has a fixed 3.6 ohm resistor on the output terminal to limit short circuit current. A separate…
Other Parts Discussed in Thread: BQ24010 Hi all,
We are having a problem with BQ24010 and TS detection. We have several production batches manufactured in different assembly houses with the same problem.
This is the schematic I'm using. Top is the outer…
Other Parts Discussed in Thread: BQ24010 I am using the following scheme .
the battery pack has protection from overcharge and overdischarge . in the case of discharge , protection disconnects the battery. If Input voltage(5V) connect Vout from BK24010 is…
Other Parts Discussed in Thread: BQ24010 I am using a c8051 to detect charger input voltage, but I have almost 3v leaking back from battery to VCC. Any help would be appreciated. My only solutions is to select a P-Channel FET to act as a on/off switch…