Part Number: BQ25170 Other Parts Discussed in Thread: BQ24085 , BQ24018 , Tool/software: Dear TI experts,
My customer uses BQ24085 and 3 diodes for their existing product.
They referred the E2E thread below. The reason why adding diods is same, for…
Hello
If the timer and termination is disabled the unit will behave similar to a current limited 4.2V power supply. BQ24013 and BQ24018 has a /TTE pin that can be used enable or disable the Timer and Termination.
This would prevent termination of…
Other Parts Discussed in Thread: BQ24018 , BQ24105 I have the following requirements for a battery charging system.
Lithium single cell charger with
Battery float voltage 4.36V or above
Charge current is 50 mA
stand alone operation
I think…