Part Number: BQ24020 Hi,
We have the pin TTE connected to the ground constantly.
I found in datasheet ,when entry timer fault condition, need toggling TTE to clear the fault, if always connect to GND, may hard to recovery.
Except that, Are there…
Part Number: BQ24020 Hello,
I can't find out POR conditions in datasheet.
I am designing the charger that battery is connectd to bq24020 alltime. I want know Timer fault reset if we disconnect power to Vac and Vusb after bq24020 detected Timer fault…
Part Number: BQ24020 Hello.
I noticed that part of Figure2(page 9) is cut off in the datasheet.
*datasheet :
Single-Chip Li-Ion & Li-Pol Charger IC w/Autonomous USB-Port & AC Adapt datasheet (Rev. E)
www.ti.com/.../bq24020.pdf
Could you give…
Hi Bill,
Thanks for your reply. This is what I thought might be happening, however, the datasheet for the BQ24020 suggests that if less than 3V is detected (as would be expected in the battery protected shutdown case) the bq24020 would attempt to do…
Part Number: BQ24020 If ISET2 (pin 7) is pulled high (charging at 500 mA) and then ISET (pin 2) is left floating, will charging still work ?
Thanks in advance
Other Parts Discussed in Thread: BQ24020 What taper current I take to calculate taper rate? In the datasheet for bq24020 charger there are 2 values for the taper current, depending what USB you are using. USB500 has 50mA taper current when USB100 has…
Other Parts Discussed in Thread: BQ24020 Hi
Hi,
I am using BQ24020 charger IC to charge 120mAh Li-ion battery. I set the charge current to around 100mA. Attached is the circuit schematic. The problem I am facing is STAT1 and STAT2 signals indicate…
Other Parts Discussed in Thread: BQ24020 Hi,
Please note that I intend to use varta EZ XL pack or similar –attached PDF file with NTC.
Q1: what is Taper timer; and USB Taper threshold mean? See page 2.
Q2: please describe how can a time out…
Hi Dick,
The WPT Tx is bq500211A (BQ500211ARGZ): * The Tx coil is Wurth 760308111 (A11)
The WPT Rx is bq51013A (BQ51013ARHLT): * The Rx coil is Vishay IWAS-3827EC-50 * The current is set for 300mA with a limit of 360mA
The battery charger IC is…