Part Number: BQ24045 I have a question about the TS terminal.
I connected the thermistor from the TS terminal to Vss to use the TS function.
And I want to use two additional functions.
But I don't know how to pulled low or driven high on…
Part Number: BQ24045 Other Parts Discussed in Thread: BQ25887 , Hello,
I have 2 21700 Li-on batteries in series for my application. I created a board using the BQ25887 which works okay, but the balancing portion isn't the best if the batteries have…
Part Number: BQ24045 Fuel Gauge PN: BQ27421YZFR-G1B
Battery Charger IC PN: BQ24045DSQR
When a FG is power cycled after running for a while will it behave identically to a FG powered up for the first time? I'd like to characterize the charge behavior…
Part Number: BQ24045 Other Parts Discussed in Thread: BQ24095 Hello Flob,
Is your issue solved or still get the same issue? Because I also get the similar type of issue in my BQ24045DSQT IC. So is there any solution so please share with me.
I get…
Part Number: BQ24045 Other Parts Discussed in Thread: BQ24040 Hi,
I just made a design with BQ24045 in order to charge a 1A battery cell. The configuration I set is the following one:
ISET = 200mA
Current terminarion threshold = 20mA
ISET2 = tied…
Part Number: BQ24045 Other Parts Discussed in Thread: BQ24040 We used BQ24045 Charging IC for the charging of 3.7V 800mAh battery (min 3V - max 4.2V). But when the battery voltage is below 4.06V and put on the charging then the CHG status pin is not changing…
Part Number: BQ24045 Other Parts Discussed in Thread: BQ25170 Hi Team,
In our design the BQ24045 receives it's power from a wireless charge receiver. We want to reduce the transmitted power as much as possible to avoid thermal issues. Everything would…
Part Number: BQ24045 According to the linked FAQ,
" Normal battery Charge -- Connected to NTC thermistor in battery pack to monitor battery temp. 50uA current source will develop a voltage that is monitored by internal voltage comparators. Charge is…
Part Number: BQ24045 Other Parts Discussed in Thread: TPS62742 , BQ24230
Dear colleague,
Our customer encounter below issues:
Background:
This is Bluetooth product that uses BQ24045 as a charging IC. and the battery is a 4.35v high-voltage lithium…
Part Number: BQ24045 Other Parts Discussed in Thread: BQ24078 Dear,
We are planning to implement BQ24045 battery charging IC in our system i have already worked on the BQ25606RGER where my charging current requirement was high.
My question is that…