Part Number: BQ24070 Tool/software: Hi,
I am currently using BQ24070 for an IoT device application. There is TS pin that is used to monitor the NTC temp of the battery. If we are not using the TS pin in our application, can it be left floating? or should…
Part Number: BQ24070
Tool/software:
Hi Garrett,
This is a follow up to my previous thread. I still have the original board with the fault. Now we are bringing up pre-production units and and now I've seen this problem appear in one of those...so a red…
Part Number: BQ24070 Tool/software: Hello!
This design has been fully tested and now we are in pre-production mode.
One particular board had the charger working, but something changed and I'm trying to exhaust all possibilities before concluding that…
Part Number: BQ24070
We're using the above design in our design. During load testing I discovered that the battery wasnt actually charging.
Stat1/2 PG is read by a micro controller and some GPIO based LEDs are currently relaying the status during…
Part Number: BQ24070 Hi again Garrett,
I have a question about DPPM as it relates to current limiting and prevention of damage to the BQ24070.
In our design, the battery is a single 18650 Li-Ion cell and the chip is powered by a 5V output AC to DC wall…
Part Number: BQ24070 Hello! We're planning to use the BQ24070 to charge a single 18650 Li-ion battery...As you know these batteries look like an overgrown AA cell...the battery in the product can be replaced by the end-user.
We are going to use a 5V…
Part Number: BQ24070 Hi Garrett,
One more question! For the case of: - no battery present. - there is a load connected to the OUT pins. - the device is powered off. - 10nF cap on DPPM As we've discussed, when the 5V is turned on to VIN, the BQ24070 will think…
Part Number: BQ24070
I built the circuit you see in the schematic
Input is 5.25V using the power supply, output voltage is 4.15 V and connected to another PCB I designed. Vbat is 4.05 V .
When I connect a Li-Ion battery to this circuit, I see that…
Part Number: BQ24070 Other Parts Discussed in Thread: TPS630250 , BQ25180 , BQ24079 , LMR51430 , BQ25181 , BQ25180EVM Hello Texas Instruments community!
I am redesigning a device and would like your help.
These are the requirements: 10Vdc – 30 Vdc input voltage…
Part Number: BQ24070 To gain additional energy capacity, we designed a board with 2 BQ24070. Each device is linked to the same voltage source (VIN1=VIN2), the same output (VOUT1=VOUT2) but manage its own battery (see simplified schematic below).
We noticed…