Part Number: BQ24070
I built the circuit you see in the schematic
Input is 5.25V using the power supply, output voltage is 4.15 V and connected to another PCB I designed. Vbat is 4.05 V .
When I connect a Li-Ion battery to this circuit,…
Part Number: BQ24070 Hi,
I am using one BQ24070 as a Power path manage IC for my battery charging and regulated power for 2G modem. (as shown in the below picture)
When the Mosfet switch turns ON, a glitch comes in the regulated output of BQ24070…
Part Number: BQ24070 Tool/software: Hello!
This design has been fully tested and now we are in pre-production mode.
One particular board had the charger working, but something changed and I'm trying to exhaust all possibilities before concluding that…
Part Number: BQ24070
Tool/software:
Hi Garrett,
This is a follow up to my previous thread. I still have the original board with the fault. Now we are bringing up pre-production units and and now I've seen this problem appear in one of those...so…
Part Number: BQ24070 Hi Garrett,
One more question! For the case of: - no battery present. - there is a load connected to the OUT pins. - the device is powered off. - 10nF cap on DPPM As we've discussed, when the 5V is turned on to VIN, the BQ24070…
Part Number: BQ24070 Other Parts Discussed in Thread: TPS630250 , BQ25180 , BQ24079 , LMR51430 , BQ25181 , BQ25180EVM Hello Texas Instruments community!
I am redesigning a device and would like your help.
These are the requirements: 10Vdc – 30 Vdc…
Part Number: BQ24070 Hi Sir,
My customer encountered a problem with the behavior of pin STAT1.
When the charger IC fully charged the battery and continued to operate overnight (maybe up to 8~10hours), they found the pin STAT1 will start to blink.…
Part Number: BQ24070 To gain additional energy capacity, we designed a board with 2 BQ24070. Each device is linked to the same voltage source (VIN1=VIN2), the same output (VOUT1=VOUT2) but manage its own battery (see simplified schematic below).
We…
Part Number: BQ24070 Other Parts Discussed in Thread: TL1963A greetings to the experts of Texas Instruments and members of the forum.
The power supply of our tracking device is designed as follows:
the processor (the system load) is made up…
Part Number: BQ24070 Other Parts Discussed in Thread: BQ25155 , BQ25601 , TPS7A25 , BQ25606 Hello,
in our current design we are using BQ24070 which has preset system output 4.4v. In the updated system we need to have 3.8v output. Could you recommend…