Part Number: BQ24072 Hi,
Some devices fails after use.
Chg pin is low , PG is low , but there is no battery charging current.
TS is OK, about 0.8v
1) Temperature during charging is very HIGH... could that damage the device permanently ?
2) Could GND thermal…
Part Number: BQ24072 Dear Sir/Madam
My customer asked to review BQ24072 schematic. Could you please review the attached schematic?
- Battery Information ; LiPo, 1 cell, 3000mA. - Supply voltage : 5V - Fast charge current : Will select one between 500mA…
Part Number: BQ24072 Hi Team,
customer is looking for a 12V/25mA common low cost linear charger. (1S)
per checked on the web I found several solution and would like to check with you any other recommendation?
Thanks!
Patty
Part Number: BQ24072 Hi TI expert
If ISET Pin is left unconnected, what will be the current consumed if it is left floating? Is there any condition for ISET setting ?Does it work properly in floating state?
Best regards,
Thomas
Part Number: BQ24072 Other Parts Discussed in Thread: BQ25155 , BQ25120A , BQ25150 , BQ21061 Hi TI team,
I have got a question about bq24072 device. I wanna use it with 3.7V Li-on battery, but the charger goes up to 4.2V.
Is it possible to somehow low the…
Part Number: BQ24072 Other Parts Discussed in Thread: BQ24075 , BQ24078 , TPS3779 Hi team,
My customer would like to add the SYSOFF function in their design, but on the board right now is BQ24072.
The reason to use this pin for preventing the over-discharge…
Part Number: BQ24072 Other Parts Discussed in Thread: BQ24074 Based on the linked question by Eric Robertson1 about the BQ24072 charging in USB100 instead of usb500 I would like to know what the root cause was if possible. Also, how can we avoid such an…
Part Number: BQ24072 Hello
I use the next scheme for BQ24072:
If I connecting input viltage(USB_5V) - BAT_PWG(PGOOD) must pull down.
But not in my cases. I have pulsation on this output
Why?
I hope for an your reply.
Thanks.
Part Number: BQ24072 Hello.
We have a classic BQ24072TRGTR configuration to have a charging current of 1.5A. With + 5V at V_USB, EN1 = 0 and EN2 = 1, a 4000mA lithium polymer battery with nothing drawing any more current, we are unable to maintain 1.5A…