Part Number: BQ24073 Tool/software: Does BQ24073 have battery reverse protection function.After reverse connection, the chip heats up and the battery is removed. The chip is connected normally and its function is normal.
Part Number: BQ24073 Tool/software: Hi
I have a TI component in the system for charging, BQ24073 and I have a problem with charging current that doesn't make any sense.
I have set current charge to 350mA and limit to 500mA. When I charge under 3V…
Part Number: BQ24073 We have a client that uses a lot uf bq24073 charge controllers in his application.
As this a linear controller, thermal considerations need to made.
Seveal hunderd units using this controller are returned with a burned up bq24073…
Part Number: BQ24073 Tool/software: Hi TI Team,
I am encountering an issue with the BQ24073 Li-ion battery management IC when trying to reset an active PCM (Protection Circuit Module) on a Li-ion battery. Here are the observations:
Setup Details…
Part Number: BQ24073 Is there any danger in operating a product we have designed that uses the BQ24073 for a PMIC with the battery removed? We are having our product safety-tested and the intended deployment will be hard-wired to power. Ordinarily this…
Part Number: BQ24073 Other Parts Discussed in Thread: BQ27220
Tool/software:
Hello,
I'm designing a battery charger using the BQ24073 IC and noticed that the KILIM and KISET factors have a wide spread in the datasheet. Question : should I use the…
Part Number: BQ24073 Tool/software: Hello,
I want to design a USB-C powered device which charges the LiPo-2000mAh Battery while powers the ESP32-S2 MCU at the same time.
I've found this BQ24073 IC but I'm not sure if this IC fits as a best solution…
Part Number: BQ24073 Hi All,
if we go through the datasheet of BQ24073 on page number 10 "Recommended Operating Conditions" Input current, IN pin is mentioned as 1.5A and the Iout current is mentioned as 4.5A.
As per general understanding if output…