Part Number: BQ24075T Other Parts Discussed in Thread: BQ24079 , BQ24079T Hi TI!
I have exactly the same question as in this thread: https://e2e.ti.com/support/power-management/f/196/p/658352/2423455 I dont understand why the minimum charge current differs…
Part Number: BQ24075T Other Parts Discussed in Thread: BQ24072T Hi all Would you mind if we ask BQ24075T? We would like to understand the function "Reverse Current Protection". We assume that Reverse Current Protection has two protections as f…
Part Number: BQ24075T Hi all Would you mind if we ask BQ24075T? How much is the minimum VBAT's voltage which Q2(FET) swtiches on? Is VBAT more than 3.2V? Kind regards, Hirotaka Matsumoto
Part Number: BQ24075T Hi Team, I calculate safety time of bq24075T and reference d/s formula. In my calculate result is 50 kohm. why d/s result is 46.8 kohm?
Part Number: BQ24075T Hello sirs,
BQ24075T RISET range is 590 ohm~ 3K ohm. But our target fast charge current is 200mA so that will exceed 3K ohm .(ˋ890/0.2 = 4.4K ohm)
Is there any problem for this ? TKS !
Part Number: BQ24075T Hi Sir
May I know
1. what's the value of VIN-DPM for BQ24075T
2. if EN2=1 and EN1=0 (Set by external resistor from ILIM to VSS) ,how much input current will be reduced?
in the datasheet ,only show USB500 for example ,have any…
Part Number: BQ24075T Hi all Would you mind if we ask BQ24075T? <Question1> If we select USB500 mode, we recognize that it is not necessary to set ILIM resistor. However, there is no ILIM resistor, it doesn't operate to charge. So, does ILIM resistor…
Hello,
It seems wired. Picture2, when OVP happens, the current should decrease to 0, but why high current overshoot could be seen in the picture? and picture 3, the current should be increased to charge current, why keep 0?
Regards
Part Number: BQ24075T Hi,
Now my customer is evaluating bq24075T EVM and then they can see unexpected behavior after SYSOFF to Low. I'd like to know this is expected behavior of bq24075T or not. This can be seen at EVM so can you try to duplicate…