Other Parts Discussed in Thread: BQ24075T
Hi, working out the resistor values for the NTC circuit
I thought I'd do the sums to calculate the resistor divider values.
My input parameters are as follows:
Vin = 4.77V
Rhot = 4.926k; 45degC threshold…
Part Number: BQ24075T Other Parts Discussed in Thread: BQ24075 , Hello,
I have an application where I might want to use the bq24075T to charge a battery at 190 mA. I noticed that the bq24075T datasheet has a specified minimum of 300 mA (R_ISET = 3 kohm…
hi
i am using this BQ24075TRGTR adn is working at the moment. but i bought a wrong part BQ24075RGTR. and am using the same circuit for the BQ24075TRGTR.
how can i modify the circuit to get it working ? i have pulled Ts down to Vss. with a 10 k resistor…
Part Number: BQ24075 Other Parts Discussed in Thread: BQ24232 , , BQ24030 , BQ24070
Dear SIr
As we know BQ24075T have first charge cycle LED indicate issue
Could you kindly help to suggest linear charger solution without this issue?
i saw BQ24232…
Other Parts Discussed in Thread: BQ24075T Dear Sirs,
Our Customer have the High/Low temp recovery point question of BQ24075T.
RD request that need the data of Min and Max for V HYS (HOT) and V HYS (COLD) of BQ24075T.
Pls help to check if BU can…
You are right that when Vin is above Vout + Vdo, Vout will be regulated to 5.5V.
If Vin is 5V, Vout = Vin - Iout*Ron. The value depends on the real dropout across the FET.
Thanks,
Wenjia
Other Parts Discussed in Thread: BQ24075T , BQ24073 Dear,
Do you know what's the Vout(reg) means as shows below, why BQ24075T 's Vout(reg) is as high as 5.5V? my understanding vout(reg)should equal to 4.2V. is't right?
another question is what 's…
Hi Franco,
I SET : is used for fast charge current programming.
I LIM : Is used for current limit programming.
What is the resistor values used in both of these pins? in your post, you are talking about current limit but you set your Iset…
Other Parts Discussed in Thread: BQ24075T Team
I am posting the following question on behalf of a customer who recently experienced unexpected behavior while using a BQ24075T device:
"
Normal
0
false
false
false
…
Other Parts Discussed in Thread: BQ24075T The BQ24075T terminates after voltage regulation mode is reached and then the charge current drops to ~ 10% of the programmed fast-rate charge current.
I have a situation where there are short current pulses…