Part Number: BQ24076 Hi TI Experts,
I'm currently using the TI USB charger BQ24076.
I would like to find a USB battery charger that able to charge the Li-Ion battery and user also to program the MCU through USB simultaneously.
Is there such product…
Part Number: BQ24076 Hello, I'm Walter
I want to develop a iot sensor device with Li-poly battery.
So, I found BQ24076 for battery charger. I will use USB port for batter charge. And my device need 5V(same as USB power).
Here is my question.
1. If…
Part Number: BQ51013B Other Parts Discussed in Thread: BQ24076 , BQ51052B , , BQ51013
Hello,
Can someone from TI applications please take a look at the attached schematic? It's devoid of any proprietary information. It's a wireless charging + fuel gauge…
Hi Ioannis,
Hardware Firmware Team Hardware Firmware Team said: At what battery voltage level Vout 4.4V drops(start decreasing or cut off)?
If the battery is the only source of power connected (VIN is not present), then VOUT will be VBAT - VDO(BAT-OUT…
Part Number: BQ51050B Other Parts Discussed in Thread: BQ24040 , , BQ24072 , BQ24076 Hi, regarding the example of Pag 32 of the bq51050B datasheet (Figure 37. Wireless Power Receiver and Wired Charger), I would like to replace the unavailable bq24040.
Would…
Part Number: BQ24073 Other Parts Discussed in Thread: BQ24075 , BQ24076 , BQ24079 , BQ24078 Dear Team,
Does BQ24073 have shipping mode?
Or I can control CE PIN pull High and enter shipping mode without VIN?
If VIN=0, VBAT is powered, will there be an output…
Part Number: BQ24202 Other Parts Discussed in Thread: BQ24196 , , BQ24076 , BQ25616 Hello,
I am planning to use BQ24202DGN as phone charger for a project.
In the data sheet it says it provides current up to 500mA. If i connect any iphone and android phone…
Part Number: BQ24010 Other Parts Discussed in Thread: BQ24076 , BQ24040 , BQ24100 Hi, I want to use BQ24010 for my design. From the application circuit, it is noted that the Charge current output (Pin) is connected to both Battery and Load together, where…
Part Number: BQ24071 Other Parts Discussed in Thread: BQ24076 , BQ24078
Hi, Could you tell me about DPPM? When the DPPM pin is floating state, Charge is disabled but OUT is output? Customer wants to interrupt the current of "IN→BAT" through the current of…