Part Number: BQ24079T Other Parts Discussed in Thread: BQ24079 , Hi Team,
What is the difference between BQ24079 & BQ24079T? View BQ24079 datasheet device comparison table of VBAT shows that BQ24079T is 6.6V?
But check the BQ24079T datasheet but it shows…
Part Number: BQ24079T Other Parts Discussed in Thread: BQ25606 For an application I would like to use the bq24079T as a charger but without the input path (>1.5A load @ 5V).
The bq24079T is used for charging (parallel), discharging and disconnecting…
Part Number: BQ24079T Other Parts Discussed in Thread: BQ24079 Hi TI!
This question is slightly related to some of the other questions in this BQ2407x group.
1) In the datasheet it says "Do not leave SYSOFF unconnected to ensure proper operation." Is it…
Part Number: BQ24079T Hi team,
The pre-charge current is set by Kprechg/Riset where Kprechg is 70(min)/88(typ)/106(max).
Is the equation still the same when in USB100 mode? (EN2=0, EN1=0)
Thanks.
Regards,
Allen
Part Number: BQ24079T Other Parts Discussed in Thread: TPS3420
Hi,
I'm trying to implement a circuit around SYSOFF function that will turn off the system output with a delay.
My current circuit looks like this:
SYSOFF is connected to MCU I/O which…
Part Number: BQ24075T Other Parts Discussed in Thread: BQ24079 , BQ24079T Hi TI!
I have exactly the same question as in this thread: https://e2e.ti.com/support/power-management/f/196/p/658352/2423455 I dont understand why the minimum charge current differs…
Part Number: BQ24079T Other Parts Discussed in Thread: BQ24232HA , , BQ24079 , BQ24072 , BQ24073 , BQ24230 HI
The customer wants to end the charge at 45 when using the bq24232HA.
I learned about BQ24079T during the search as below.
However, it is difficult…
Part Number: BQ24079T Hi TI! Related to this post: e2e.ti.com/.../656891 Is the quiscent current of the BQ24079T higher than 6.5uA during SYSOFF when there is load on the OUT pin? I see in the datasheet that the test condition for the 6.5uA is given during…
Part Number: BQ24072T Other Parts Discussed in Thread: BQ24072 , BQ24075 , BQ24075T , , BQ24079T , BQ24079 Hi,
Would you be able to share the differences between the BQ24072T and the BQ24072? Do these changes also apply to the BQ24075, BQ24075T, BQ24079 and…