Part Number: BQ24080 Hi Team
If I would like to recommend customer to use our CHARGER! 1. How do I know when to recommend Linear or Direct or Switch mode Charger?
2.Could you share what deference between Linear / Direct / Switch mode Charger ?
Thank…
Part Number: BQ24080 Other Parts Discussed in Thread: BQ25180 Hi Team,
Good day! I'm posting this on behalf of the customer.
Here it is:
I am using your BQ24080DRCR to charge a 4.2V lipo battery. I want to charge the battery iven if it is connecter…
Part Number: BQ24080 Other Parts Discussed in Thread: BQ24081-Q1 , Hi Team,
I saw the datasheet about BQ24081-Q1 and it has BQ24080-Q1.
But I can' t search it in ti.com.
Do we have Q1 version about BQ24080?
Hello
A theory we are investigating.
The TPS61022 operating in PFM mode (MODE Low) at light load will operate in a burst type of mode. Switching burst to charge output capacitor with low current between the burst.
BQ24080 has a long termination deglitch…
Part Number:
The deep discharge of a LiPo batterypack with integrated PCM does not recover with the BQ24080, but instead shows strange sawtooth discharge behavior.
We slowly discharged a LiPo battery pack with integrated PCM. Once the battery was…
Part Number: BQ24080 Hi,
We are using BQ24080 in one of our project to charge 5.2AH Li-ion battery. When we start charging and it reaches to constant current mode (between 20% to 80% charge cycle) it gives current in the range of 400-500mA, whereas it…
Part Number: BQ24253 Other Parts Discussed in Thread: BQ24080 , Hey there,
I have a question about the functionality of these kind of charging chips. Let's say my system is powered on and I am charging a LiPo at the same time. Now I wonder what will happen…
Hi Luis,
Thank you for your advice.
I was looking into the Battery protectors, specifically into the Front-End, cause otherwise, these protectors need separate cell information.
So in our case, we will use a 3-cell LiPo 11.1[V]. I will need a Battery…