Part Number: BQ24090 It is found that when some products are charged, the charging value of the first 10 seconds is only half of the preset current value, and about 10 seconds later, the charging is normal. An oscilloscope was used to capture the voltage…
Part Number: BQ24090 Other Parts Discussed in Thread: BQ24091 , BQ24092 , BQ24093 , BQ25170 Hi,
Kindly suggest the Alternate Part's for BQ24090 (Direct Replacement) , without any modification in the design/ footprint.
Thanks and Regards,
Kavitha
Part Number: BQ24090 Hi team,
Issue: using the BQ24090, it was found that some products were charging with only half the pre-set current value of the first 10S charging, and after about 10S charging, it became normal. Grabbed the NTC voltage value with…
Part Number: BQ24090 dear
It is found that when some products are charged, the charging value of the first 10 seconds is only half of the preset current value, and about 10 seconds later, the charging is normal. An oscilloscope was used to capture…
Part Number: BQ24090 Dear ones shalom
we are using the device and in few occasions we have high temperature in the BQ24090 during charging
we use ISET with 2KOhm and ISET2 is LOW PRET has 2K Ohm resistor
the over temperature is during charging of empty…
Part Number: BQ24090 Dear Sir/Madam,
i am using the below circuit for BQ24090.
IN:ADAPTOR_5V
OUT: V_BAT connect to battery parallel with system load.
PG, CHG connect to MCU
TS connect to battery NTC and MCU CHARGE_OFF for recovery.
BTW, I try to trigger…
Part Number: BQ24090 Other Parts Discussed in Thread: BQ24074 ,
Hello,
I found that the BQ24074 is used in this Adafruit module as a solar charger: learn.adafruit.com/.../design-notes . Note that one of the main reasons they use this module is because of…
Part Number: BQ24090 Other Parts Discussed in Thread: BQ24092 , Hi team,
For bq24092 with Jeita, the charging current at 0 ~ 10 degree will be half the Iset.
however, for bq24090 without Jeita, what will be the charging current between 0 ~ 10C? Should it…
Part Number: BQ24090 Other Parts Discussed in Thread: BQ25171-Q1 I would like to power the BQ24090 with a regulated 12 Volt DC wall adapter. I read the specifications, but there appears to be some confusion as whether this can be done. On Figure 2, the…