Part Number: BQ24095 Hello Sir/Madam,
Nice to E-meet with you,
One of my battery charging application i use bq24095 charging IC for charge battery as per bellow specification:
Battery: single Lithium-ion 3.7V battery
Battery capacity: 1400mAH
Charge Rating…
Part Number: BQ24095 We use BQ24095 and VBUS in the charging circuit. The battery is fully charged and the system load is 0.3A. If we suddently remove the USB Cable, we can observe the Battery voltage is drop from 4.3V to 3.6V for 0.3ms. Then the Battery…
Part Number: BQ24095 Other Parts Discussed in Thread: BQ24075 , The product folder of BQ24095 mentions that the device supports power path. Is it similar to the power path available in BQ24075 where the system is isolated from the battery?
Part Number: BQ24095 Hello Sir,
First i want to introduce with my charging circuit with reverse battery protection unit.
Issue: When i charge my battery in the right way there will be ok but when i change the polarity of battery then charging…
Part Number: BQ24095 Hi, Team
We have a problem of bq24095 for terminate current when charge cycle be completed.
In figure of charging profile, after the Iout meet the terminal threshold, it should be cut off. We found an issue that the CHG pin changed…
Part Number: BQ24095 Hello Team,
We are working on one project and we are selected BQ24095 battery charger , for our application.
We have listed below query
1. What is the behavior of BQ24095 charger, if user insert "dead battery" for charging…
Part Number: BQ24095 Hi, Team
Customer has a project that selected BQ24095 as system charger.
We have a question to thermal protection.
If the temperature over 45C, charger occur hot/cold fault, the charger will be terminated.
Then the temperature lower…
Part Number: BQ24095 Hello Team,
We are working on one project and we selected BQ24095 Charge controller for charging battery.
kindly review the attached schematic of BQ24095, and give your valuable suggestion on it.
Battery Specification - Li-ion, 3.7V…
Other Parts Discussed in Thread: BQ24095 , BQ24095EVM-005 , BQ24090 Hello,
Could you review attached schematic and let me get the result?
And there are some question
1. If there is any problem when it booting without Battery?
2. When 1A charging current…
Other Parts Discussed in Thread: BQ24095 Hi Sir
I have a question of BQ24095 could you hlep to explan, When battery absent (Battery detect mode), does system (OUT pin) current limit follow the Iset setting or just 10mA.