Part Number: BQ24100
Dear Forum Members,
I am currently designing a board for a battery charger using the BQ24100 Charger IC. I would like to know if it is recommended to connect PGND and Earth directly. Please let me know.
Thank you and regards, …
Part Number: BQ24100 I am having the same issue. Boards with BQ24100 return from the field with TS pin having low impendence to ground (100 ohms) or input to ground shorted AND output to ground shorted. Did the post a couple years ago get resolved? …
Part Number: BQ24100 Other Parts Discussed in Thread: BQ25620 , BQ25616 , BQ25798 Hi team,
Is there any newer device than BQ24100 which has 2 status pin and can discern full charge or battery absense without I2C?
It would be better if there was also Powerpath…
Part Number: BQ24100 Other Parts Discussed in Thread: BQ24133 Dear Expert
The STAT pin of the charging chip BQ24133 encounters the following problems:
When only the adapter is connected without the battery, the STAT level changes and the STAT pin LED flashes…
Part Number: BQ24100 Other Parts Discussed in Thread: BQ24104 , BQ24103 , BQ24090 , BQ24040 , BQ24041 , BQ24210 Sir
I want to know the difference between the bq2410DQCR and bq2410DQCT, I want to use bq2410 ic for a circuit but I got confused when came into…
Part Number: BQ24100 I am looking for the footprint of the above mentioned IC that can be downloaded to PCB123, 2D CAD, Eagle or other downloadable version.
Leonard Roque
Isolux llc sr. engineer.
We are preparing the paper work today. Do you have any thoughts on why the TS pin on this BQ24100 part would get damaged in the circuit after weeks to months in the field. There is nothing connected to this pin that the end user can touch since the…
Part Number: BQ24100
Hi everyone!
I have a problem.
When the input voltage is + 5V, the battery does not charge When the input voltage is less than + 5V, the battery is charged.
I take schematic from datasheet (calculate only resistor on SET1 and SET2…