Part Number: BQ24100 I have implemented the bq24100 as attached and can not get it to charge. Vin is 5.25V, Vbat is 2.67V (18650 cekk), TS is 1.58V, CE is low. PG led lights, but Stat1 and Stat2 are off. Same input and battery on eval module charges just…
Part Number: BQ24100 Other Parts Discussed in Thread: BQ24210 Hi,
What is the internally set termination current for a ICHG < 250 mA?
I have a 350 mAh battery but with a fast charge restriction to 0.5C so ICHG is 175 mA. In the Jan 15 datasheet, Electrical…
Part Number: BQ24100 Team,
in our application with bq24100 (single 18650 cell), it sometimes occurs that both the IC itself and also the output current sense resistor (100mOhm) are getting damaged in the moment when the battery (cell) is being soldered…
Part Number: BQ24100 Other Parts Discussed in Thread: BQ24105 , BQ25606 Hello,
I am a bit new to this site and question I have is in regards to using the BQ24100 or BQ24105 as a stand alone charger for a customer.
Main idea is would like to charge their…
Part Number: BQ24100 Hello Everyone,
As we are using BQ24100 for our battery management.
1) STAT1 and STAT2 are both indicating high(1.1 Volt) while charging.
2) While charging STAT2 goes high STAT1 will be low.
Please suggest what might be issue?
circuit…
Part Number: BQ24100
I am having a problem with a BQ24100 charger I would like to some guidance on. On a normal functioning unit the charger turns on and chargers as expected then turns off and decays until the recharge threshold is reached when it turns…
Hi Kumar,
I understand what happened with the bq24010, the input voltage is directly proportional to the heat loss on the linear regulator.
As for the bq24100, yes, it looks like a switch on the TTC is necessary to reduce current consumption when battery…
Part Number: BQ24100 Dear BMC team,
One customer reported below issues when experimenting bq24100EVM.
For his application, customer may connect battery to the ouput of bq24100 while no voltage is applied at input.
In such case, he measured high peak…
Part Number: BQ24100 OK this is my send time around . I am performing FA on our home charger for one of our electronic monitoring devices. we have been getting them back form the field with burnt up boards and the chips are pretty much destroyed. I have…