Part Number: BQ24120 Other Parts Discussed in Thread: BQ24104 , BQ24109 , BQ24103 Can you confirm that the only difference between BQ24120 and BQ24104 are the following?
Pin 2 - STAT1 (behavior) - BQ24120 – either ON or OFF - BQ24104 – either ON or…
Part Number: BQ24120 Hello, On page 24 of the datasheet, ISET 2 resistor is computed through the equation in number 5. The VISET2 voltage used in the equation is 1.0V. However, in the electrical characteristics table, VISET2 is 100mV.
Can you please advise…
Hi Jeff
Sorry, missed your earlier replies. Yes, the problem was a soldering issue. Thanks for your help, though.
And in answer to your question, this application needs a single LiPo cell of about 1000mAh, and a charging current of less than 0.5A. The…
Hi,
can this device (or others) be programmed to charge 3 NiMH cells in series (3 x 1.2V=3.6V).
Do we have any other completely integrated switching solution? Thanks
Umberto
Other Parts Discussed in Thread: BQ24120 Hi TI TEAMS
I have two questions for BQ24120 application
1.If the TS pin is not used in the application, it should be connected to GND through 10kΩ pulldown resistor ??
2. Can I adjust the temperature for this range…
Other Parts Discussed in Thread: BQ24120 Hello ,
I am using BQ24120 in my design.
attached is the image files of schematics and footprint.
I am facing an issue while 5V is supplied through V_SOLAR.
i am getting only .7V at V_SOUT, without connecting battery…
Other Parts Discussed in Thread: BQ24120 Hi E2E forum
We are designing a charger using the bq24120 IC.
Can the VTSB be supplied externally or must we use the internalle generated supply?
The internally generated TS bias voltage has a 10 % regulation…