Part Number: BQ24158BQ24158 (register05 bit5 reset to 1) Special Charger register in charging IC will be reset to 1 (low charge current) when device entry standby mode and wait over 5 sec then wakeup.
Does TI know what condition will cause the register05…
Part Number: BQ24158 Hi,
We are using the battery charger BQ24158FFT in our design. Our targetted charge current is 100mA and we are using the Rsns as 820mE. But it is only taking 30 mA as charging current.
Below is the register configuration maintained…
Part Number: BQ24158 Hi,
We are using the battery charger BQ24158FFT in our design. We are planning to use it in OTG mode also. But, when it switches to OTG mode - it is draining around 800 to 900mA from battery even in no load condition. Hope you can…
Part Number: BQ24158 Hi,
We are planning to use BQ24158YFFR in our design as the Battery charger. As per my understanding from the docs, we can either operate the Battery charger in 15mins mode or 32 secs mode. But in both modes, the system MCU has…
Part Number: BQ24158BQ24158YFFT I2C register write and read issue.
We found the write data and read data are not the same and below is my write/read process, register and data.
1. Write BQ24158 register 0x02, data 0xb6,
2. Read Bq24158 register…
Part Number: BQ24158 Hi team,
Currently we are working on this battery charger and we are not able to change the register values and set our required charging voltage and charging current values.
Below is the schematics we are following.
We have…
Part Number: BQ24158 Other Parts Discussed in Thread: BQ24155 Hello,
i have a customer who needs support with the BQ24158 and wrote the following:
"We have long saga with the BQ24158.
The yield of our product is very bad and after very long…
Part Number: BQ24158 Hi,
My customer is wondering if the I2C interface can also used 3.3V pull up?
Will there be any risk using 3.3V pull up?
Since 1.8V is mentioned in our datasheet but customer is having 3.3V at their host side.
Great thanks…
Part Number: BQ24157 Other Parts Discussed in Thread: BQ24158 , Hi Team,
My customer using both ICs and according to the datasheets, both have the same slave address (7 bit):
0b110101 1
But, both only respond to 0b110101 0 can you please clarify…
Part Number: BQ24158 Dear,
My application is APD and now want to use TI BQ24158. I can only found Linux Driver in Web. But my system is Android 7.0, So Could you kindly help provide Android Driver Source Code? Great thx.