Other Parts Discussed in Thread: BQ24161 Hello Team,
We are Planning to use BQ24161 Battery charger for charging 3.7V, 1050mAh Li-ion battery, by USB and External DC jack.
As we explore BQ24161 seems to be suitable for our application, we have few query…
Other Parts Discussed in Thread: BQ24161 , BQ27530-G1 , BQ27530EVM , BQSTUDIO I am using the bq24161 in a circuit. I have a battery charge LED connected between the STAT pin and the DC IN pin via a 120 ohm resister. The issues I am experiencing are:
The…
Other Parts Discussed in Thread: BQ24161 , BQ24251 , BQ24250 Hi,
Anybody knows what's the máximum current the chip may supply in the SYS pin when?:
1.- There's no battery connected?.
2.- There's a battery charging (Vbat < Vminsys)?. …
Other Parts Discussed in Thread: BQ24161 Hi,
I am using BQ24161 as a BATTERY CHARGER with power management. I am connecting DRV with TS as shown in attached file. I could not enable the charging process. It shows battery temperature fault from status register…
Other Parts Discussed in Thread: BQ24161 , BQ24161EVM-721 , BQ24160 I am using the BQ24161EVM-721 evaluation board for the BQ24161. Using the GUI provided by TI, I can see that the charger is charging the battery from USB even though that I don't actually…
Other Parts Discussed in Thread: BQ24161 Quick overview of what I'm trying to do:
I'm working on a design where a BQ24161 is used for charging the battery and power path management. If the system is shut down, a downstream regulator is turned off,…
Other Parts Discussed in Thread: BQ24161 I am using the BQ24161 Battery Charger with Power Path Management. It is configured as per the Figure 4 of the TI datasheet. As of yet I have not written any code to support the I2C interface. When I leave the device…
Hi
I have question regarding bq24161 the DM pin is NC pin. but it is not written if it should be connected to gnd or left open.
in the bq27530 EVL it is connected to usb. in my design the controller is connected to usb so I dont want to connect it.
can…
Other Parts Discussed in Thread: BQ24161 Hi,
When I am using the BQ24161 with an AC adapter I get a fault condition over the VSYS (See attached)
Every time a battery detection cycle starts the VSYS falls and the VBAT looks corrupted.
It doesn't happen when…
Other Parts Discussed in Thread: BQ24161 No battery connected to VBAT of BQ24161, to make VBAT output a regulated voltage, TE bit should be set to 0 to disable charging termination. In datasheet, VBAT=4.2V in this condition. But we found very bit ripple…