Other Parts Discussed in Thread: BQ24167 Below is written on datasheet 9-page.
"bypass BAT to GND with at least a 1μF capacitor."
Please let me know about Max capacitance vaule.
Best regards,
Satoshi
Other Parts Discussed in Thread: BQ24167 Dear all.
Do you have the definition of time output to DRV(LDO) pin from the voltage inputted into IN pin or USB pin of bq24167?
Regards, PAN-M
Other Parts Discussed in Thread: BQ24167 , TPS2500 HI,
I am using BQ24167RGET dual input charge in my design.
In both charging & discharging phase i am hearing hum sound.
I am suspecting the noise is generated by the inductor.
As per reference design…
Other Parts Discussed in Thread: BQ24167 , BQ24165 Hi
I have one question for BQ24165 / BQ24167 Current Half Function,
These device Charge current Min is 550mA.
But these device has Current half mode.
1) BQ24167 => JEITA Function 0.5C at temp…
Other Parts Discussed in Thread: BQ24167 , BQ24165 Hi
I had this question for last time.
Thank you very much , I understood this spec.
>I have one question for BQ24165 / BQ24167 Current Half Function,
>These device Charge current Min is 550mA. …
I can't have the battery charger, BQ24167, consume 30uA when the battery is connected and Vin and Vusb are 0V.
Do you have a recommended circuit layout that would cut power from the battery to the battery charger but allow the battery to power the…
Other Parts Discussed in Thread: BQ24167 , TPS2500 Hi,
I am using BQ24167 dual input charger IC & TPS2500 USB Boost converter in my charger design.
I am able to hear HUM sound from the system.(Mostly near Input section of TPS2500 )
Block Diagram:-
…
Other Parts Discussed in Thread: BQ24167 Hi,
I have a li-po battery charger design using BQ24167. I am facing issue with power good status. The power good pin is toggling continuously in following condition.
Battery voltage is 3.19 V
Charging using USB…
Other Parts Discussed in Thread: BQ24167 hi,
i am using BQ24167 in a solar charger. I disabled the TS input by connecting the DRV out of Bq24167 to TS input. So i didn't use thermal protection for battery charging.
When i am testing my board for solar…
Other Parts Discussed in Thread: BQ24167 hi,
i am using BQ24167 battery management IC to charge a battery pack.
My Question is: I set current limit for both AC_IN and USB_IN as 2.5 and 1.5 respectively, if i connect a 5V, 1 A adapter as source, will the…