Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: BQ24167 My customer is working through several technical issues and needs to know what is the revision of the BQ24167 if the date code is 231 ?
Other Parts Discussed in Thread: BQ24167 Dear Team,
We have got an opportunity of BQ24167 from Sambon electric which is targeting a Bluetooth speaker to JVC in Japan market.
According to BQ24167's datasheet, IC supply current TYP is 15mA.
The customer…
On one of the posts, following circuit was shown for sharing of Battery Thermistor input between Battery charger and Fuel gauge:
The post said "From what I found in the literature the best solution is to connect the thermistor to the fuel gauge and use…
Part Number: BQ24250 Hi Team,
I have a question about bq24250 behavior. I described the detail behavior in attached powerpoint but could you support below questions?
bq24250_tech_question.pptx
[background] When VBAT is in between VBATREG and VBOVP(VBAT…
The default charge voltage is 3.6V and 1000mA so if are you not periodic resetting the watchdog, the charger should charge the battery to 3.6V with 1000mA max charge current. To charge to 4.2v, you would need to enter host mode using I2C writes. Try…
Other Parts Discussed in Thread: TPS630252 , TPS62180 , BQ24167 , TPS630250 , TPS63051
How can I connect 2 TPS630252 outputs together to provide double current capability?
Thank you,
Peter
bq24165 is the only dual input, standalone switchmode charger we have. If you need USB compliance than you might need to add a bq24392 to help determine where to set the IUSBx pins. We also have a dual input linear charger, bq2403x family.
If one input…
Other Parts Discussed in Thread: BQ24167 I have two designs that are using the BQ24167 device. When I connect the DC source to the IN line the PG and CHG LEDs light up. If there is a battery the CHG LED will go off some time later, presumably after a initial…