Part Number: BQ24170 Hi ,
I am using BQ24170 in designing my battery charging circuit. The battery i am using has 2 cells 7.4V and 10000mAh spec with 3 connectors( battery charging , discharging port and a battery balancing connector). I need help connecting…
Part Number: BQ24170 Hi,
I am using 3.7V/cell nominal volatge(4.2V/cell max voltage) Li ion and 3000mAh/ cell capacity cells in 2s3p configuration. Can i configure the CELL pin like two pin configuartion(Float) even though have used 3 cells parallel…
Part Number: BQ24170 Tool/software: Hello Teams,
When the charger is charging the battery, what the status will be of pin 19 /BATDRV on the BQ24170?
When the power adapter is plugged in, I want to set the power path to the system and charge the…
Part Number: BQ24170 Pls help to provide the CMRT 6.6 and EMRT 2.11 for below TI product.
LM3478MAX/NOPB
BQ24170RGYR
OPA333AIDBVR
RMI_CMRT_6.6.xlsx RMI_EMRT_2.11.xlsx RMI_EMRT_2.11.xlsx
Part Number: BQ24170 I have a system with BQ24170 where I expect charge current to be:
Rsr= 10mR
Viset = 0.43V
Ichg = 0.43 / (20*10m) = 2.15A
However, it's only about 1.5A. If I increase Viset to 0.59V it is 2.15A, but then it should be 3A according…
Part Number: BQ24170 Tool/software: Dear TI Support,
We are using the BQ24170 battery charger IC in our design, and would appreciate your assistance with two issues we’ve encountered during prototyping and testing.
️ Project Overview:
Input…
Part Number: BQ24170 Tool/software: dears,
my customer using bq24170 with below schematic diagram
when cell pin connect to 3.3v to high.
Add 3s cells can't charging, but STAT show charging with no 3s LI-CELL.
Part Number: BQ24170 Other Parts Discussed in Thread: BQ25750 , BQ25730 Tool/software: Hi team,
Can you suggest a best alternative for 3S charging? Thanks!
Requirement:
1. 3S1P, Li-on
2. 12,V, 15V adapter
3. Power management path
4. 3A for…
Part Number: BQ24170 Hi
The TS pin is OF BQ24170 is connected to resistors including a NTC 10kohm RESISTOR / THERMISTOR in order to prevent high temperature of the battery.
Is it right to attach it to the battery? If it is attached to the BQ24170…