Part Number: BQ24192 Other Parts Discussed in Thread: LM3478 Hello,
We are using the BQ24192 on one of our client's boards to charge 3.7V, 1S12P lithium ion battery pack. Following is the power tree that we have on board,
Battery (3.4-4.3V) --> Boost…
Part Number: BQ24192 Other Parts Discussed in Thread: BQ24190 , , Tool/software: Hello, the datasheet for this device states: For safe operation, the bq24190, bq24192, bq24192I has an additional hardware pin on ILIM to limit maximum input current on ILIM…
Part Number: BQ24192 Other Parts Discussed in Thread: BQ25628 , BQ25622 Tool/software: We are in the process of evaluating a new model using BQ24192 and are experiencing the following problem.
<Problem> The Charge Termination Current is set to 128 mA…
Part Number: BQ24192 Other Parts Discussed in Thread: BQ27531-G1 , , BQSTUDIO , USB2ANY , EV2400 Hello,
We are using BQ24192 charger with BQ27531-G1 gas gauge. Our gas gauge controls the charger by enabling the GG_CHRGRCTL_ENABLE command. As per the…
Part Number: BQ24195 Other Parts Discussed in Thread: BQ24192 , Tool/software: Hello Ti Support Team, Kindy explain me difference between BQ24195 vs BQ24192.
Part Number: BQ24192 Tool/software: Hello, I'm planning to design a USB - PD power delivery system for the below requirements.
Sl No
Requirements
1
Input power
2
Power Adapter
5V/3A , 9V/3A, 12V/3A, 15V/3A
3
Power Bank…
Part Number: BQ24192 Hi Team, I'm using BQ24192 PMIC for one of our projects. I'm using a 3.7V Li-Ion (18650) battery and I need to set the charge current to 512mA which is the minimum value as per datasheet. So, I changed the default value, 0x60 of the…
Part Number: BQ24192 Hello Team,
We are using a BQ24192 battery charger in our system with the following configurations.
- The Battery is connected to the output of BQ24192 with an additional fuse in the series.
We are facing an issue with the…
Part Number: BQ24192 Other Parts Discussed in Thread: BQSTUDIO
Hi,
we use in our project the bq24192 as a charger for 1Cell-LiIon Battery.
I set externally at ILIM Pin a resistor (R=180 Ohm) to set the charging current to approx. 3A.
When i…
Part Number: BQ24192 Other Parts Discussed in Thread: BQ25731 , , TPS61230 , BQSTUDIO Hi,
we use in our project the bq24192 as a charger together with bq25731 as a gasgauge.
Almost everything working fine but i'm just wonder that when VBUS=0 and…