Part Number: BQ24193 Tool/software: Hi Team, Please validate the attached circuit, here i have used 12V as input to BQ24193 to act as a power part + if no input it should work with Battery Input. I want to understand that if the input is 12VDC what is…
Part Number: BQ24193 Tool/software: Hi Team,
We are using BQ24193 for battery charging and for generating main board power 3.3v via LDO. The main input power supply is 12v and our board requires < 200ma @ 12v input.
On some of our boards, this 3.3v…
Part Number: BQ24193 Other Parts Discussed in Thread: DRV8210P Tool/software: Hi Team,
In my design, I have used BQ24193 in order to charge the Battery capaciity of 3.7V, 13400 mAH 1s4P with 5V,2A as a input. Could you please validate desgin as per…
Part Number: BQ24193 Other Parts Discussed in Thread: BQ25792
Tool/software:
I'm using the BQ24193 to charge Li-ion cells. It's a bit overkill since I'm only using it for a cell charging system, but I'm using this IC due to other practical considerations…
Part Number: BQ24193 Hello, I'm using BQ24193RGET Battery charger IC and I can see the below mentioned problems.
A DC electronic load (with 2.5A) is connected on the (VSYS) of the charger IC without battery.
CASE 1: When the Load is turned "ON" and…
Part Number: BQ24193 Other Parts Discussed in Thread: BQ24292I , BQ25672 , BQ24192 , BQ25892
The sourcing situation for BQ24193 is difficult. We are therefore looking for alternative parts. Preferred is something pin compatible.
1. Is BQ24193 the…
Part Number: BQ24193
Sometimes our product goes over 45c during charging. In that situation the JEITA voltage limit of 4.05v kicks in. We have observed that during charging, if the battery is already over 4.05v when the 45c boundary is crossed, the…
Part Number: BQ24193 Other Parts Discussed in Thread: BQ27531-G1 Hi,
Could you please confirm about the working for bq24193 on bq24193 + bq27531-g1 solution?
A fully-discharged pack (Battery voltage = almost 0V) is attached to bq27531-g1 BAT pin and…
Part Number: BQ24193 Other Parts Discussed in Thread: TPS3831 , TPS3840 , TPS3890 , TLV803E
Hi,
We are working on BQ24193 BMS IC.we need a battery monitoring circuit for bq24193 for battery protection.we need to cutoff the batfet when battery voltage…