Part Number: BQ24195L Other Parts Discussed in Thread: BQ24195 Hi Team,
My customer has some questions on the BQ24195L (after transiting from the BQ24195).
The specification shows that the maximum output current (Isys) of BQ24195L is 2.5A and Ibat…
Part Number: BQ24195L Hello,
As part of my project code, on initialization I am forcing the Charger IC chip to detect the source of input by setting high the 7 bit of the REG07. (regardless of DC source presence)
However the detection flag stays on…
Part Number: BQ24195L Hi Team,
The customer is asking that is it fine to put a current sense amplifier across the resistor to monitor the charging current? Or is there any other way to get the charging current information? Thank you.
Best regards…
Hey Elie,
There are several timing issues here.
1) When VBUS is connected to the BQ24195L charger, it will try to detect the type of USB port it is connected to based on the USB BC1.2 specification.
2) When VBUS is connected to your phone, it likely…
Part Number: BQ24195L hey,
I am using the BQ24195L to detect the nature of the device that is connected to my phone.
So I have connected the phone to my host pc using a usb cable (by only connecting the D+ and D- pins) , and i have used a splitter…
Part Number: BQ24195L Hi,
My customer is doing test on BQ24195L. They found there is a 30uA leakage current from battery to device after full charging ( using high-resolution multimeter), they wonder where is this current come from? which function is…
Part Number: BQ24195L Other Parts Discussed in Thread: BQ24190 , BQ24195 Hi,
My customer is checking with me, if no battery load, How many current SYS pin can provide? I'm not sure if device will be in a HIZ without battery, or, just treat it as a buck…
Part Number: BQ24195 Hi All,
We have some questions about the output current of SYS PIN of BQ24195L.
The specification shows that the maximum current of ISYS is 2.5A, and the Ibat discharging maximum continuous current is 6A, we would like to know…
Other Parts Discussed in Thread: BQ24298 , BQ24195L , BQ25616 I would like to have suggestions for single cell LiPo battery charging ICs that are similar to BQ24195L/BQ24298 for the application of GSM/cellular internet connectivity. The main feature required…