Part Number: BQ24196 Other Parts Discussed in Thread: BQ24192 Hi Team,
My customer now use BQ24196.
When they connected with battery, it is normal and no voltage dropped.
When they don't connect with battery, SYS has a voltage dropped when 3.3V power…
Part Number: BQ24196
Hi Team,
When customer setup a charging limit voltage by REG04, if the voltage is close to this limit voltage setup by REG04, will the chip change from fast charge to Constant voltage charge?
Thanks!
Part Number: BQ24196 Other Parts Discussed in Thread: BQ24192 Is it possible to disable the use of TS1 and TS2 inputs (ie not connect them to thermistors/resistor network), as we are controlling the charger remotely that also monitors the battery temperature…
Part Number: BQ24196 Dears,
I am currently using the BQ24196 for charge and discharge management in my device. The registers I set are as follows, REG00=0X37; REG01=0X1E; REG02=0X49; REG03=0X11; REG04=0XC3; REG05=0X88; At present, 6 boards with BQ24196…
Part Number: BQ24196 Hi,
I want to know the quiescent current through BATFET when high-z mode is disabled and no VBUS, while the BATFET is on.
Is there any big difference for the quiescent current between disabling and enabling high-z mode?
Part Number: BQ24196 Hello E2E,
Please let me know about OTG operation for BQ24196. When switch the mode from charge to OTG 5V output, is it necessary to change REG [5:4] from 0:1 to 1:0? Is it impossible to control by simply switching the OTG pin logic…
Part Number: BQ24196 hello
my bq24196 work normal when battery on; l set the shipping mod and take the battery away; my sys output dispeared; l insrert the battery and connect the input ;there is still
no outout; whant`s wrong with it ? does the bq24196…
Part Number: BQ24196
Hi,
In customer's production line they had tested short protection fuction in OTG mode. The OTG output is from VBUS pin rather than PMID pin.
Test procedure is
a) Putting the bq24196 in OTG mode and check the output voltage…