Part Number: BQ24210 In the datasheet SLUSA76B at chapter 8.4.5.6 it is noted: "An external resistor on the ISET pin is used to program the output current (50 to 800mA) and can be used as a current monitor ."
How can the actual monitor current…
Part Number: BQ24210 Hello Guys,
Good day.
Need your advise if the BQ24210DQC is suitable for the photovoltaic panel with below specifications:
Pmax (W) = 5W Voltage at Pmax (V) = 18.1 V Current at Pmax (A) = 0.29 A Open voltage circuit (V) = 22.2 V
photovoltaic…
Part Number: BQ24210 Hi
Designing in a solar charger (single 18650) using BQ24210. According to data sheet Typical Application, leaving V_DPM unconnected will enable Battery Tracking Mode which is optimum. Downstream components (connected to BAT) have…
Part Number: BQ24210 Other Parts Discussed in Thread: BQ24650 , TIDA-00049 Hi team,
my customer need a solar charger with system power monitor and power path management. The charge currenti is 500mA
I find the BQ24210 or BQ24212 may meet this requirement…
Other Parts Discussed in Thread: BQ24210 Hello all,
I have a customer who is looking for an alternative to the BQ24210 to charge a single LiIon cell with Dual Input Support, OVP/UVP Protection, or both features combined. Are there any devices and reference…
Part Number: BQ24210 I was wondering if anyone had experience using this charger with a 2 cell lipo pack where the cells are in parallel. I assume that his would be fine since it would be like one large 1 cell battery.
Part Number: BQ24210 Is there a way to charge the external battery pack with BQ24210.
I don't know how to connect a TS pin that requires NTC WIRE from BATTERY on BQ24210.
Is the only way to take the LI-ION battery out and use it after disassembling…
Part Number: BQ24210 Dear TI Experts,
I designed a solar charger circuit with a 6V/1W solar panel for a 2200 mAh Li-ion battery. Based on Fig. 13 Typical Application Schematic (on page 20 of SLUSA76B), I use LPCM (therefore connect TS to VTSB, no thermistor…