Part Number: BQ24230 Other Parts Discussed in Thread: BQ51013 , BQ51013B Hi,
Customer want to question regarding their application. The customer want connect both IC in their application, please see details below.
I have some questions about a product…
Part Number: BQ24230 Dear TI,
I have developing the Battery charge with BQ24230.
Our device is that payment terminal and there are inside battery(3.7V, 920mAH).
We also need the compliance to USB-IF Standard, that's why i choose the BQ24230.
Problem…
Part Number: BQ24230 Other Parts Discussed in Thread: BQ24232 , BQ25723 Hi, I designed a car battery operated device, with BQ24230RGTT. As per the data sheet maximum input voltage 28V . I assumed that BQ24230RGTT will can operate at 24V or 12V vehicles…
Part Number: BQ24230 Hello,
We use the Charger BQ24230. We have to decrease the quiescent current of the whole system to reach an acceptable storage time of the device.
We measure a quiescent current around 13uA from Charging IC under following…
Part Number: BQ24230 Is there a way to configure the BQ24230 for device shipping? Does it have a ship mode where it latched the battery until power is supplied to VIN?
I need a 4.2V ~350mA charge lipo part with integrated PCM and power path management…
Part Number: BQ24230 How to calculate the current consumption (Icc) of BQ24230.
IN pin: Nothing is connected. BAT pin: 3.7V. OUT pin: A load carrying 100uA of current is connected.
Part Number: BQ24230 Other Parts Discussed in Thread: BQ25155 Hi Team,
Good day, we received query from customer asking the following regarding BQ24230. Kindly check list below.
"We are using bq24230 li-ion battery charger from TI. Is there any recommendation…
Part Number: BQ24230
Hi Team, The datasheet shows recommended RILIM value is 3.1k~7.8k ohm. On the other hand, my customer is using 3.0k ohm. Is it no problem? Best Regards, Yaita / Japan disty
Part Number: BQ24230
Dear TI Team,
I am working on embedded wearable device powered with 300mAh Lithium battery.
We are updating device design from prototype to consumer-grade. Currently, we are redesigning the battery related components to meet…