Part Number: BQ24230 Other Parts Discussed in Thread: BQ76920 , , BQ25071 Hi Team,
Can we use BQ24230 to charge US26650FTC1A LFP/Gr from Murata? How do we connect it to BQ76920?
Regards,
Danilo
Part Number: BQ24230 Hello.
We are currently evaluating BQ24230 for a product using single-cell Li-Polymer battery and USB power, and have encountered an issue with charging. We are using a custom board, and I've attached relevant part of the schematic…
Part Number: BQ24230 Hello,
According to the bq24230 data sheet ABSOLUTE MAXIMUM RATINGS, the maximum battery output current (continuous) is 1700mA.
My circuit typically has an average current draw about 15mA with occasional 2 second intervals of…
Part Number: BQ24230 Our product uses the BQ24230 battery charger IC. I’m looking into scaling up our production testing of our PCBs and I’m seeking some advice on how to test the BQ24230 in a production setup. Obviously connecting to a real battery takes…
Part Number: BQ24230 Hello,
we have the BQ24230 on our board to recharge a battery, after sometime the CHG led from steady on state starts blinking, but the datasheet says only that it should be either on or off. If we disconnect and reconnect the power…
Part Number: BQ24230 Other Parts Discussed in Thread: CC2642R We have two module for BQ24230 application , one is with battery and the other is non-battery .
With battery, our system boot fine.
But without battery condition, our system boot failed…
Part Number: BQ24230 Can we get some input on the expected operation of BQ24230, we are a little confused by the datasheet?
The part is already a consumer device presently in DFM but we are new to the team. Thanks in advance!
---
USE-CASE #1 (TWO…
Hi Ken,
I would say the clearest advantage for a standalone is that it is configurable in some settings through resistors while the I2C device will typically need a host device such as a micro-controller to configure the same settings or more.
Part Number: BQ24230 Other Parts Discussed in Thread: BQ24075T , BQ21040 Hi All,
During charging, INTC is sourced to TS and the voltage at TS is continuously monitored. If, at any time, the voltage at TS is outside of the operating range (V COLD to…
Part Number: BQ24230 I'd like to check about the correct treatment when we don't use the following pins.
(1) /PGOOD: Do we need care leave open or connect to GND?
(2) /CHG: Do we need care leave open or connect to GND?
(3) TS: The datasheet describes…