Part Number: BQ27750EVM-837 Other Parts Discussed in Thread: BQ24232 Dear Sir or Madame,
the following problem occurs with the gas gauge IC BQ27750 and the charger IC BQ24232 but we also encountered this problem before with different chargers and gas…
Part Number: BQ24075 Other Parts Discussed in Thread: BQ24232 , , BQ24030 , BQ24070
Dear SIr
As we know BQ24075T have first charge cycle LED indicate issue
Could you kindly help to suggest linear charger solution without this issue?
i saw BQ24232…
Hi Bill,
Thanks for your reply.
I've verified the following.
1.) The charger that I'm currently using is BQ24232 as the following silkscreen "4232HA TI 64I AFSG" is indicated on the IC itself.
2.) The connection of IC thermal pad is being connected…
The bq24232 is designed to charge up to 4.2V voltage, which is the maximum charge voltage for most LiIon/Polymer batteries. If you have a different LiPo battery that has a lower maximum charge voltage per the datasheet, you cannot use the bq24232. Can…
Hi Kazuya,
Regarding Q1, the lowest precharge current for this EVM is 128mA.
Regarding Q2 and Q3, we do not have switching charger that is suitable for this low of charge current. I recommend linear chargers like BQ25100 if you do not need power…
Mohak,
What PCB software are you using? If you want to bypass the DRC, we can help you on that with Altium.
If you are running into limitations with the board vendor, you could possibly take a look at the BQ24232 along with a standalone DC-DC converter…
Other Parts Discussed in Thread: BQ24232 , BQ51003 , BQ25100 , TIDA-00318 Hello,
I am working on a receiver design for wireless power using the BQ51003 and battery charging using BQ24232. I originally wanted to use the TIDA 00329 solution, but need…