Part Number: BQ24250 Hi Team,
The customer report that there will be a current spike when the BQ24250 switch from its linear to PWM mode when the VBAT crosses Vsysmin at around 3.3 to 3.4V.
We know this is the expect behavior. Can the team help to advise…
Part Number: BQ24250 Hi,
We are currently working on a new design containing the BQ24250. T he location of the 5V and GND charging pins on the PCB are 42mm apart from each other. Is this OK or do they need to be positioned right next to each other?
Thanks…
Part Number: BQ24250 Other Parts Discussed in Thread: BQ25601
Hi ,
I have strange conditions with BQ24250, which hangs I2C line.
I have a project , which includes BQ24250 (Charger) , STM32L4R5 (MCU) , 3 x CY3866LTI(PSoC) and bq27421(fuel gauge) , all together…
Part Number: BQ24250 Hi Team,
I have a question about bq24250 behavior. I described the detail behavior in attached powerpoint but could you support below questions?
bq24250_tech_question.pptx
[background] When VBAT is in between VBATREG and VBOVP(VBAT…
Part Number: BQ24250 Hi Team,
The customer is asking that is there any concern to set the VDPM to 4.2V as the minimum value of the GUI?
However, the minimum operating range is 4.35V in the DS, please kindly help to advise. Thank you.
Best regards…
Part Number: BQ24250 I am trying to set up the B24250 to be stand-alone compatible with a micro usb type b. How do I configure pins EN1 and EN2 if I want it to be stand alone?
Part Number: BQ24250 Hi,
I am using battery charger circuit using BQ24250 for one of the project.
After applying 5V input at input pin of charger IC getting output voltage after 10-15sec at VSYS.
Also if we are remove input from the chrager IC and giving…
Part Number: BQ24250 Hi Team,
The customer had the question about the STAT pin behavior, according to the DS description below:
Status Output. STAT is an open-drain output that signals charging status and fault interrupts. STAT pulls low during charging…