Other Parts Discussed in Thread: BQ24250C Hello~
In the page 30 of bq24250c's datasheet, Register #3 B[1:0] is described the EN1/EN0 pin status.
But, bq24250c does not have the EN0 pin. bq24250c just has EN2 pin instead of EN0.
Is the "EN1/EN0"…
Gordon,
Unlike our other chargers, this charger's TS function can be disabled if you take V(TS) above the disable threshold below:
If you do not want that functionality, check out the BQ24250C.
Regards,
Jeff
Hi Ricardo,
Thanks for your feedback.
My battery is lithium polymer with nominal voltage of 3.7V and fully charged voltage of 4.2V.
Actually I don’t need the D+/D- detection since I have found some workaround idea.
In order to be more clear I’ll…
Hi Linhong,
I have the same low Vin rise issue with the BQ24250C. I try your tip to add a 1k resistor at the LDO output. I no more see this issue on the BQ2425x test board but I still have this issue on my product prototype. May you have another tip to…