Part Number: BQ24296M Other Parts Discussed in Thread: BQ24296 Hello,
I'm not sure to understand the datasheet of bq24296M
In chapter 7.3 "Recommanded operation conditions" i read:
Isys - Output current (SYS) - 3.5A max
Ibat - Discharging…
Part Number: BQ24296M Hello,
I've searched in the data sheet but didn't find a clear answer: is there any sort of protection against battery connected in reversed polarity?
I'm asking this because I've to design a wireless remote control and…
Part Number: BQ24296M Hi
The customer design with BQ24296M. In the charging state, the chip heats up very seriously, and the surface temperature reaches 53°.
The internal temperature rises to 40° due to the handheld device. Is this temperature normal…
Part Number: BQ24296M Other Parts Discussed in Thread: BQ24296 Hi team,
Here's an issue from the customer may need your help:
BQ24296 is used for battery management. When the battery is almost full: "The actual battery voltage is around 4v-4..1v"…
Part Number: BQ24296M Hi Team,
Issue: bq24296M System Status Register REG08 - CHRG_STAT status toggling between Fast Charging and Charge Termination Done
Setup: VIn - DC Adapter(5.0 to 5.2V)/2A Battery type - 4.2V ICHG - 512mA Average System Current - 370mA…
Part Number: BQ24296M Other Parts Discussed in Thread: BQ25601 Hi,
We are using bq24296M battery charger in our design. We came across an issue with battery charger when the battery is completely drained.
Scenario:
1. Charge the battery with VIN - 5V
…
Part Number: BQ24296M We are using the BQ24296M IC when we are soldering on board, Inductor one of the line shorting with the ground. we cant find a reason for that. please suggest to me any solution is there.
Part Number: BQ24296M Dear Sir,
I found some issue that cannot quit shipping mode.
Here is the description.
1. After entering and exiting the transportation mode many times, it will happen that the shipping mode cannot be exited.
2. plug DC input(12V)…
Part Number: BQ24296M Hi I need to use BQ24296M in boost mode to power part of my device, but in this time user can connect external USB power source to input of the BQ24296M . What will do BQ24296M in this case? It will automatically disble boost mode…