Hi,
I have connected I2C & GND pins of BQ24297EVM-021 with Arduino. Where J2 connector is connected with the battery (BAT+ = battery +ve and GND = Battery -ve). Rest all the jumpers are in the same state as mentioned in the datasheet.
Battery Voltage…
Part Number: BQ24297EVM-021 Other Parts Discussed in Thread: BQ24297 , EV2400
Hello,
We are considering using the BQ24297 in our product. We would first need to evaluate the chip with the evaluation board BQ24297EVM-021 . However can we use it with…
Hi All
I am facing problem in charging battery by BQ24297EVM-021 .
Hardware configurations are :
Connected a 5V DC 2.1 A charger on J7
Battery ( 3.7V 2100 mAh) with ammeter in series on J2 ( BAT+ & GND).
INSTALLED : JP3,TS2,TS1,JP5,JP7 , JP2…
Unfortunately Roger,
I was not able to duplicate the issue on our Evaluation Module, even with all the information you provided.
The closest I was able to replicate was issue was with a lot of extra capacitance on Vsys (around 220uF), but that only…