Part Number: BQ24298 Other Parts Discussed in Thread: BQ24295 I am trying to use BQ24298 to replace BQ24295.
PMID on BQ24298: is it not intended to provide a power to another device?
When the OTG enable bit is selected (REG01 Bit 5), does it keep the…
Part Number: BQ24298 Hi,
I see in 7.3 of the BQ24298 datasheet, it says the recommended maximum for SYS output current is 3.5 A.
I am wondering if it is safe to temporarily push above 3.5 A when operating with battery and without DC source. In this case…
Part Number: BQ24298 Dear Community,
any help here is greatly appreciated.
The system
We have a handheld device and very typical usag. Use on battery power until it is dead. Charge. Repeat. We hava a single cell LiPo and the BQ24298 controller. With a…
Part Number: BQ24298 Other Parts Discussed in Thread: DP83TD510E Hi Team, seeking some assistance.
will suppy 5V@3A through USB-C and I connected to VBUS but I don't know if I have to coonect PMID to VBUS or leave it open. The DP83TD510E is an ultra-low…
Part Number: BQ24298 Other Parts Discussed in Thread: BQSTUDIO , EV2400 , BQ24296 Hi there,
I was having some difficulty with a power management circuit I am testing which uses the BQ2492RTWR chip.
When connecting the LiPo battery, there is no charging…
Part Number: BQ24298 Other Parts Discussed in Thread: BQ24296M
Hi Team, I would like to get your help regarding the customer situation with part of their design using BQ24298.| They use the BQ24298 controller in their mobile devices. After the assembly…
Part Number: BQ24298 Other Parts Discussed in Thread: BQ24296 I desgin a power source for my GSM based device. My device is works with 5V DC input and 18650 liion battery back-up.
I need to charge if batter is not full. and need an output of 3V8 (for…
Part Number: BQ24298 Other Parts Discussed in Thread: BQ24296M
Hello TI experts,
My customer consider BQ24298 for their product, so please review the schematic below.
and let me know if there are something to modify.
and here are few questions;
1.…
Part Number: BQ24298 Hi support team,
My customer is testing the BQ24298EVM. They used the resistor 220R between ILIM pin and ground. According to the engineer, bq enter HIZ mode automatically every time they plug the charger in. Input current limit is…