Part Number: BQ24314 Hi,
We got a question from customer about bq24314. Could you help us?
[Question] They need to consider failure mode of the IC. They would like to make sure failure mode of the condition that over voltage (such as 50V) is applied to…
Other Parts Discussed in Thread: BQ24314 Our customer is concerned about device operation at pin to pin short condition. They would like to know the dvice operation when ILIM pin is shorted with OUT pin or VBAT pin. How does the device operate?
If current…
Those are fine parts, but more detail on what you want to accomplish needed to pick specific parts.
bq24040 is a simple charger, bq24072 and bq24032a are power path parts. Not sure you need bq24314.
You need to post any gas gauge questions is their forum…
Other Parts Discussed in Thread: BQ27510-G2 , BQ24030
Hello Everyone,
I'm building a portable device that runs of 3.3V. I'm planning to use this battery http://uk.farnell.com/gp-batteries/nta2710/battery-li-ion-3-7v-4400mah-1s1p/dp/1848660
I…
Part Number: BQ24314A Other Parts Discussed in Thread: BQ24314 , Hi
I'm currently working on a project using the BQ24314.
The input voltage comes from a USBC interface, and given that the USBC standard has been updated to support higher power/voltage…
Part Number: BQ24080 Other Parts Discussed in Thread: BQ24314 , TPS61022 Hi, I'm using a bq24080 connected directly after a BQ24314 and the charge done state nerver come up even if the battery is full charge. However the charge conditions are met : I…
The bq2970 is not meant to work outside of the battery pack, and we don't really have a good solution here. You could try looking into using the bq24314 or one of those devices. They are meant to be placed inbetween an AC/DC wall adapter and a charger…
The schematic looks good and the PG pin can be floated if you don't need the power good indication feature.
Bq24080 is usually paired with our front end protection IC bq24314. Please refer to the below user guide.
www.ti.com/.../sluu291a.pdf
I…
Hi Avi,
Do we have lower Rds(on) OVP IC and feature is like bq24314?
My customer thinks bq24314's Rds(on) value is too big for their application.
Thanks
paul